Part Number: TM4C1294NCPDT
I want to use the functionality of DMA-Controller to transfer data from the UART-FIFO to another memory location.
The Problem is the channel assigment of the DMA-Controller to the peripherals.
I want to use the UART2 and UART4 peripheral the same time, because it is given on a board which can't be modified.
But there is no possibility beside the re-initialization of the DMA-Controller with another channel-assignment encoding.
So I am here to be inspired how to use UART2 and UART4 in DMA-Mode simultanously.
I could be also an idea like, say, to link or remap the UART4-FIFO to another peripheral, which can be used in FIFO-Mode together with the UART2 peripheral in the same channel assignent encoding.
with regards
Ali Naseri, Germany