Part Number: TMDXRM57LHDK
Hello,
I am attempting to run a test case on the Hercules RM57L843 board through VectorCAST, but the execution seems to crash / hang. I am using a Blackhawk XDS560v2 System Trace Emulator as an external debugger. The code has been compiled using the arm-none-eabi-gcc compiler, and compiles successfully. When adding --verbose to the execution command, the stdout from the execution of the test case ends with the following:
CortexR5: GEL Output: Memory Map Setup for Flash @ Address 0x0 due to System Reset Loaded FPGA Image: /opt/ti/ccsv8/ccs_base/emulation/drivers/../../common/uscif/./dtc_top.jbc CortexR5: GEL Output: Memory Map Setup for Flash @ Address 0x0 due to System Reset waitUntil: RETURN load: Program load successful getBoolean: ENTRY ID: AutoRunToLabelOnRestart getBoolean: RETURN true waitForHaltIfPropertySet: Waiting for halt waitUntil: ENTRY timeout: infinite
The Red ERR LED is not lit on the development board, and the S1, S2, S3, and 5V LEDs on the Blackhawk XDS560v2 are lit.
I'm not sure if the linker script is not correct, or if it is some other issue. The stdout --verbose does indicate that the program load was successful (see above).
Has anyone experienced a similar issue before?
Thanks,
Daniel