Other Parts Discussed in Thread: TMS570LC4357, HALCOGEN
Hi all,
I am using the TMS570LC4357 Controller with the Debugger XDS200. I have the following program lines of code:
PINMUX_GIOA0_DMA_ENABLE(OFF);
PINMUX_GIOA1_DMA_ENABLE(OFF);
PINMUX_GIOA2_DMA_ENABLE(OFF);
PINMUX_GIOA3_DMA_ENABLE(OFF);
PINMUX_GIOA4_DMA_ENABLE(OFF);
PINMUX_GIOA5_DMA_ENABLE(OFF);
PINMUX_GIOA6_DMA_ENABLE(OFF);
PINMUX_GIOA7_DMA_ENABLE(OFF);
PINMUX_GIOB0_DMA_ENABLE(OFF);
PINMUX_GIOB1_DMA_ENABLE(OFF);
PINMUX_GIOB2_DMA_ENABLE(OFF);
PINMUX_GIOB3_DMA_ENABLE(OFF);
PINMUX_GIOB4_DMA_ENABLE(OFF);
PINMUX_GIOB5_DMA_ENABLE(OFF);
PINMUX_GIOB6_DMA_ENABLE(OFF);
PINMUX_GIOB7_DMA_ENABLE(OFF);
These program lines are used to program the register PINMUX[175] up to PINMUX[178]. I expect the following value for the register:
PINMUX[175] = 0x01010101
PINMUX[176] = 0x01010101
PINMUX[177] = 0x01010101
PINMUX[178] = 0x01010101
But if I look in the Debugger Output I see following values:
If I look in the Memory Map for PINMUX[175], address 0xFFFF1FCC (Base Adr. 0xFFFF1C00U + Offset PINMUX[175]. 0x3Ch = 0xFFFF1FCC) it shows me the fifth value of register PINMMR171. But the value is the right one.
It looks to me as if the display of the register data has shifted. Could you agree my observation.
Best regards
Lars