This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team
My customer just wants to know that whether LAUNCHXL2-570LC43 can support both MQTT and MODBUS communication.
Thank you.
Hello,
LAUNCHXL2-570LC43 has built-in ethernet PHY and RJ45 ethernet connector, and 570LC43 supports 10/100MHz ethernet MAC (EMAC). There is no problem to use this device for IoT application if the IoT devices are connected through a wired connection.
If wireless connection is required, you can use CC3x (for example CC3100) launchpad + LAUNCHXL2-570LC43.
This launchpad can be used for MODBUS over TCP/IP.