Part Number: TMS320F28379D
Other Parts Discussed in Thread: C2000WARE
Hi,
So I am new to F28379d and I am trying out examples on launchpad for developing a program and I am facing the issue that when RAM sharing is active between 2 cores ,the cores aren't retaining the program after power reset.
The process I follow for programming the cores is:
Setting the configuration(i.e. choosing as per need RAM/FLASH/STANDALONE) in properties for the project and first debugging it to the core-1 after which I use connect target for core-2 and Load the program out file in the core 2 .After which I click resume for both cores individually to run both .
Here's a brief description of what I have tried out for your reference :-
So, I was trying out Blinky_dc and RAM_management programs in examples for TMS320F28379d in c2000ware version 3_03 as well as 3_04.
1) Blinky_dc program works fine in both debugging (CPU1- flash & CPU2-flash) and standalone modes : - (CPU1 - standalone configuration and CPU2-flash mode). So the program is functional even in power reset case in standalone mode
2) Moving on to RAM_management program, I tried the same approach of CPU1-standalone and CPU2-flash mode but it fails on power reset and I need to keep working in debug mode(CPU1-flash mode CPU2-flash mode )and thus use jtag to program the cores every day for testing.
I need a solution to this so that both the cores can be functional after power reset even when ram sharing is active between the cores. Please do let me know the needed corrections for solving this issue.