Part Number: TMS320F28388D
Hi,
I am using CCS V10, with TI v18.12.0.LTS compiler.
I have multiple executable files in EABI format like file1.out, file2.out, file3.out. Each executable file will be loaded separately into different flash sectors via JTAG. I need to combine all the individual executable files into a single executable file, so that it can be loaded at once using CCS. I have the following questions:
1. Does the c2000 hex utility supports merging of multiple executable files into a single executable files? If yes, please provide details about how to do it?
2. Does c2000 hex utility has a provision to calculate the CRC for the input executable file image and can overwrite the CRC value at a specified address in the output executable file?
Best Regards
Amulrass V