Part Number: TMS320F28375D
Other Parts Discussed in Thread: SYSCONFIG,
Sysconfig seems to only support the 176 pin and 337 pin packages for the TMS320F28375D but the 100 pin package is missing. Is there a way to get this to work?
Regards
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F28375D
Other Parts Discussed in Thread: SYSCONFIG,
Sysconfig seems to only support the 176 pin and 337 pin packages for the TMS320F28375D but the 100 pin package is missing. Is there a way to get this to work?
Regards
6th Sep is a holiday in US and hence please expect a delay in response.
The 100 pin package is the same as the F2807x package. For now, you can use that while we add the support to SysConfig.
Nima
Thank you. If I choose the F2807x for the project, how can I change the processor back in code composer? Certainly I can generate the files in one project and copy the generated files to another project. Is there a way to stay in one project?
Regards
SysConfig and Project Properties go hand in hand. I am working on the fix and I will send you a version when I'm done so you can have it all in one project under F2837xD.
Nima
Neil, what is your CCS version and inside the CCS install folder, what is your sysconfig version?

Paste the content I gave you and merge it into the folder:
ccs\utils\sysconfig_1.9.0\dist\deviceData\F2837xD
make sure the JSON file I sent replaces the JSON file you have.
Nima
I added the files but I get this error on an existing sysconfig project.

I also created a new project and added sysconfig to the new project and got a different error. In both cases only the 176 and 337 versions of the chip appear.
Thats a strange error. I would revert back to see if the error is removed. I think you need another file updated as well which I cannot provide at this time. I have this approved by the team and should be available in CCS11.1.
Nima