Part Number: TMS320F28375D
Other Parts Discussed in Thread: C2000WARE, SYSCONFIG
Tool/software:
Hello!
Device: F28375D
C2000Ware version: 5.01
CCS version: 12.6.0.00008
I have an existing single core (cpu1 only) project with Sysconfig generating various files. This project uses .project +.cproject files, NOT .projectspec.
I am trying now to now split this project into two cores. I have created two different .syscfg files, one with --context "CPU1" and the other with --context "CPU2". I tried two methods:
1) creating a single project with two different build configurations. CPU1 configuration excludes the CPU2 syscfg. CPU2 configuration excludes CPU1 syscfg.
2) creating two projects, one for CPU1 and one for CPU2, each with their corresponding syscfg files.
In both cases, I'm having the following issues:
a) clocktree.h doesn't get generated by the CPU2's syscfg, the CPU2 project does not have access to clock constants.
b) ipc / interrupt settings show warnings, indicating that the settings cannot be checked correctly without the context of the other CPU.
c) I cannot see the CPU1 and CPU2 tabs to allow editing multi-core syscfg mode. I see many online resources referencing these tabs.
These problems all seem to be caused because the 2 syscfg files do not seem to be aware of each other.
I noticed that in all of the dual core example projects I have seen, .projectspec files are used to define two separate projects (CPU1 and CPU2) in the same .projectspec file.
Are we required to use the .projectspec file, with two separate projects for each CPU, in order to use syscfg in dual-core mode? Or can we use the .project + .cproject files (either 1 project with 2 configurations, or 2 separate projects)?