Part Number: TMS320F28375D
Tool/software:
Hi,
I've got a bit complex EV dual-core application working on a custom board.
The application work well but once a week (more or less) the mcu seems to freeze. The only possible solution to restart it is a complete power cycle.
Please, can anyone suggest me a method to catch this bug?
At the very first I need to discover if it's an HW problem, and then I need to catch the max possible infos about the last operations happened before the mcu hang.
I also use a big amount of variables continuously exchanged between 2 core.
Are there some papers, documents to study?
Thx in advance.