Hi,
I am trying to flash a custom F2812 board. The boot mode is H0. But during entering debugging, I receive the following error:
C28xx_CPU1: Failed CPU Reset: (Error - 1137@ 0x7). Device held in reset.
Please note the following:
1. I am able to get success in the JTAG integrity test.
2. When booted in H0, the XRS pin shows pulse wave. It shows 3.3 V only for 4.6ms and then is at 0V for 500ms, in a cyclic behaviour.
3. When booted in Flash / SCI mode, XRS shows 3.3V all the time.
4. I have used latest CCS with XDS110.
5. I have used the ezdsp_ram_f2812 linker file.