Part Number: TMS320F2812
Hi,
To go into the F2812 bootloader, my understanding is to set GPIO F2, F3, F4 and F12 to the proper state and turn on power. Alternatively, I have circuitry which is able to set these GPIO pins to the proper state in SW. Is it then possible to jump to bootloader from SW? If so, what address would I need to jump to? Is there any HW settings or resets one should perform before jumping to the factory bootloader through SW? I am specifically looking to leverage the onboard SCI-A bootloader. Thank you.