Part Number: TMS320F28379D
I am trying to use the EPWM module to generate double pulse waveforms for driving a power FET test rig. Based on my understanding of this controller family, the appropriate way to do this is in software using interrupts (ie INT_EPWMx) that are triggered by the timebase counter being equal to some CMPx - this should correspond to a rising or falling edge of the PWM waveform.
I am currently stuck on getting two pulses of different widths to repeat in a periodic fashion (pulse 1 has width a, and pulse 2 has width b). I am trying to do this by changing the duty cycle of the EPWM back and forth from one value to another. Forcing the EPWM low for isolated double pulses is a problem I will solve later - probably via trip zone interrupts.
Here is a minimal version of the logic I would like to implement - this is based on the epwm_ex11_configure_signal example in c2000 ware.
#include "driverlib.h"
#include "device.h"
#include "board.h"
uint32_t epwm1IntCount;
EPWM_SignalParams pwmSignal1 =
{10000, 0.5f, 0.5f, true, DEVICE_SYSCLK_FREQ, SYSCTL_EPWMCLK_DIV_2,
EPWM_COUNTER_MODE_UP_DOWN, EPWM_CLOCK_DIVIDER_1,
EPWM_HSCLOCK_DIVIDER_1};
EPWM_SignalParams pwmSignal2 =
{10000, 0.25f, 0.5f, true, DEVICE_SYSCLK_FREQ, SYSCTL_EPWMCLK_DIV_2,
EPWM_COUNTER_MODE_UP_DOWN, EPWM_CLOCK_DIVIDER_1,
EPWM_HSCLOCK_DIVIDER_1};
// Interrupt Prototype
__interrupt void modDutyCycle(void);
void main(void)
{
// Initialize needed components
epwm1IntCount = 0U;
Device_init();
Device_initGPIO();
Interrupt_initModule();
Interrupt_initVectorTable();
Board_init();
SysCtl_disablePeripheral(SYSCTL_PERIPH_CLK_TBCLKSYNC);
EPWM_configureSignal(myEPWM1_BASE, &pwmSignal1);
// Set EPWM
EPWM_configureSignal(myEPWM1_BASE, &pwmSignal1);
SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_TBCLKSYNC);
//Interrupts
Interrupt_enable(INT_EPWM1);
EPWM_enableInterrupt(myEPWM1_BASE);
EPWM_setInterruptSource(myEPWM1_BASE, EPWM_INT_TBCTR_D_CMPA);
EPWM_setInterruptEventCount(myEPWM1_BASE, 1U);
Interrupt_register(INT_EPWM1, &modDutyCycle);
EINT; // Enable Global interrupt INTM
ERTM; // Enable Global realtime interrupt DBGM
for(;;)
{
asm ("NOP");
}
}
__interrupt void modDutyCycle(void)
{
if (epwm1IntCount > 0U)
{
EPWM_configureSignal(myEPWM1_BASE, &pwmSignal1);
epwm1IntCount = 0U;
}
else
{
EPWM_configureSignal(myEPWM1_BASE, &pwmSignal2);
epwm1IntCount++;
}
EPWM_clearEventTriggerInterruptFlag(myEPWM1_BASE);
Interrupt_clearACKGroup(INTERRUPT_ACK_GROUP3);
}
This works if I modify the duty cycle for the first time to the new value and stop cycling through the interrupts (I get pulse width b), but if I continue cycling the EPWM stops outputting any signal at all as measured on an oscilloscope. I have looked through the program flow using breakpoints in debug mode and confirmed that my EPWM_INT_TBCTR_D_CMPA is indeed being properly triggered and cleared each cycle, and that the logical flow of my program snippet is correct.
What am I missing here? Is the configure signal function in ex11 doing something I'm not aware of/something not appropriate for implementing this? This is seems to be an issue stemming from being unfamiliar with this family of controllers as opposed to a fundamental logic/programming problem.