Part Number: LAUNCHXL-F28379D
Hello,
I am trying to generate a double pulse signal using the EPWM module and I am unable to generate a PWM signal that's less than 1.5Khz. My target frequency is somewhere between 50hz to 100hz, but when I tried specifying it as a variable, the launchpad generates no signal.
PFA my code
#include "F28x_Project.h"
//
// Defines
//
#define Dutycyc 0.5
#define Frequency 0.1 // kHz
#define Phase_shift 10
#define RP_pulse 20 //100 ns
#define EPWM_CMP_UP 1
#define EPWM_CMP_DOWN 0
//
// Function Prototypes
//
void InitEPwm1Example(void);
void InitEPwm2Example(void);
void InitEPwm3Example(void);
void ShutEPWM(void);
void EnablePWM(void);
unsigned int PWM_Enable =1;
unsigned int First_time = 1;
__interrupt void epwm1_isr(void);
__interrupt void epwm2_isr(void);
//
// Main
//
void main(void)
{
//
// Step 1. Initialize System Control:
// PLL, WatchDog, enable Peripheral Clocks
// This example function is found in the F2837xD_SysCtrl.c file.
//
InitSysCtrl();
EALLOW;
ClkCfgRegs.PERCLKDIVSEL.bit.EPWMCLKDIV=0;
EDIS;
//
// Step 2. Initialize GPIO:
// This example function is found in the F2837xD_Gpio.c file and
// illustrates how to set the GPIO to it's default state.
//
// InitGpio();
//
// enable PWM1, PWM2 and PWM3
//
CpuSysRegs.PCLKCR2.bit.EPWM1=1;
CpuSysRegs.PCLKCR2.bit.EPWM2=1;
// CpuSysRegs.PCLKCR2.bit.EPWM3=1;
//
// For this case just init GPIO pins for ePWM1, ePWM2, ePWM3
// These functions are in the F2837xD_EPwm.c file
//
InitEPwm1Gpio();
InitEPwm2Gpio();
// InitEPwm3Gpio();
//
// Step 3. Clear all interrupts and initialize PIE vector table:
// Disable CPU interrupts
//
DINT;
//
// Initialize the PIE control registers to their default state.
// The default state is all PIE interrupts disabled and flags
// are cleared.
// This function is found in the F2837xD_PieCtrl.c file.
//
InitPieCtrl();
//
// Disable CPU interrupts and clear all CPU interrupt flags:
//
IER = 0x0000;
IFR = 0x0000;
//
// Initialize the PIE vector table with pointers to the shell Interrupt
// Service Routines (ISR).
// This will populate the entire table, even if the interrupt
// is not used in this example. This is useful for debug purposes.
// The shell ISR routines are found in F2837xD_DefaultIsr.c.
// This function is found in F2837xD_PieVect.c.
//
InitPieVectTable();
//
// Interrupts that are used in this example are re-mapped to
// ISR functions found within this file.
//
EALLOW; // This is needed to write to EALLOW protected registers
PieVectTable.EPWM1_INT = &epwm1_isr;
PieVectTable.EPWM2_INT = &epwm2_isr;
// PieVectTable.EPWM3_INT = &epwm3_isr;
EDIS; // This is needed to disable write to EALLOW protected registers
//
// For this example, only initialize the ePWM
//
EALLOW;
CpuSysRegs.PCLKCR0.bit.TBCLKSYNC = 0;
EDIS;
InitEPwm1Example();
InitEPwm2Example();
EALLOW;
CpuSysRegs.PCLKCR0.bit.TBCLKSYNC = 1;
EDIS;
//
// Step 4. User specific code, enable interrupts:
//
//
// Enable CPU INT3 which is connected to EPWM1-3 INT:
//
IER |= M_INT3;
//
// Enable EPWM INTn in the PIE: Group 3 interrupt 1-3
//
PieCtrlRegs.PIEIER3.bit.INTx1 = 1;
// PieCtrlRegs.PIEIER3.bit.INTx2 = 1;
// PieCtrlRegs.PIEIER3.bit.INTx3 = 1;
//
// Enable global Interrupts and higher priority real-time debug events:
//
EINT; // Enable Global interrupt INTM
ERTM; // Enable Global realtime interrupt DBGM
//
// Step 5. IDLE loop. Just sit and loop forever (optional):
//
for(;;)
{
asm (" NOP");
}
}
//
// epwm1_isr - EPWM1 ISR
//
__interrupt void epwm1_isr(void)
{
//
// Update the CMPA and CMPB values
//
//update_compare(&epwm1_info);
//
// Clear INT flag for this timer
//
if (PWM_Enable == 0 )
ShutEPWM();
else
EnablePWM();
PWM_Enable =0;
EPwm1Regs.ETCLR.bit.INT = 1;
//
// Acknowledge this interrupt to receive more interrupts from group 3
//
PieCtrlRegs.PIEACK.all = PIEACK_GROUP3;
}
//
// epwm2_isr - EPWM2 ISR
//
__interrupt void epwm2_isr(void)
{
//
// Update the CMPA and CMPB values
//
//update_compare(&epwm2_info);
//
// Clear INT flag for this timer
//
EPwm2Regs.ETCLR.bit.INT = 1;
//
// Acknowledge this interrupt to receive more interrupts from group 3
//
PieCtrlRegs.PIEACK.all = PIEACK_GROUP3;
}
//
// epwm3_isr - EPWM3 ISR
//
//
// InitEPwm1Example - Initialize EPWM1 configuration
//
void InitEPwm1Example()
{
//
// Setup TBCLK
//
Uint32 EPWM1_TIMER_TBPRD = 200000/Frequency/2;
Uint32 EPWM1_CMPA = EPWM1_TIMER_TBPRD*Dutycyc;
EPwm1Regs.TBPRD = EPWM1_TIMER_TBPRD; // Set timer period 801 TBCLKs
EPwm1Regs.TBPHS.bit.TBPHS = 0x0000; // Phase is 0
EPwm1Regs.TBCTR = 0x0000; // Clear counter
//
// Set Compare values
//
EPwm1Regs.CMPA.bit.CMPA = EPWM1_CMPA; // Set compare A value
//
// Setup counter mode
//
EPwm1Regs.TBCTL.bit.CTRMODE = TB_COUNT_UPDOWN; // Count up and down
EPwm1Regs.TBCTL.bit.PHSEN = TB_DISABLE; // Disable phase loading
EPwm1Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1; // Clock ratio to SYSCLKOUT
EPwm1Regs.TBCTL.bit.CLKDIV = TB_DIV1;
EPwm1Regs.TBCTL.bit.SYNCOSEL =1;
//
// Setup shadowing
//
EPwm1Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW;
EPwm1Regs.CMPCTL.bit.SHDWBMODE = CC_SHADOW;
EPwm1Regs.CMPCTL.bit.LOADAMODE = CC_CTR_ZERO; // Load on Zero
EPwm1Regs.CMPCTL.bit.LOADBMODE = CC_CTR_ZERO;
//
// Set actions
//
EPwm1Regs.AQCTLA.bit.CAU = AQ_SET; // Set PWM1A on event A, up
// count
EPwm1Regs.AQCTLA.bit.CAD = AQ_CLEAR; // Clear PWM1A on event A,
// down count
//
// Active Low PWMs - Setup Deadband
//
EPwm1Regs.DBCTL.bit.OUT_MODE = DB_FULL_ENABLE;
EPwm1Regs.DBCTL.bit.POLSEL = DB_ACTV_HIC;
EPwm1Regs.DBCTL.bit.IN_MODE = DBA_ALL;
EPwm1Regs.DBRED.bit.DBRED = 20;
EPwm1Regs.DBFED.bit.DBFED = 20;
//
// Interrupt where we will change the Compare Values
//
EPwm1Regs.ETSEL.bit.INTSEL = ET_CTR_ZERO; // Select INT on Zero event
EPwm1Regs.ETSEL.bit.INTEN = 1; // Enable INT
EPwm1Regs.ETPS.bit.INTPRD = ET_1ST; // Generate INT on 3rd event
}
//
// InitEPwm2Example - Initialize EPWM2 configuration
//
void InitEPwm2Example()
{
//
Uint32 EPWM2_TIMER_TBPRD = 200000/Frequency/2;
Uint32 EPWM1_CMPA = EPWM2_TIMER_TBPRD*Dutycyc;
Uint32 EPWM2_CMPA = EPWM1_CMPA+Phase_shift;
Uint32 EPWM2_CMPB = EPWM2_CMPA-RP_pulse;
// Setup TBCLK
//
EPwm2Regs.TBPRD = EPWM2_TIMER_TBPRD; // Set timer period 801 TBCLKs
EPwm2Regs.TBPHS.bit.TBPHS = 0x0000; // Phase is 0
EPwm2Regs.TBCTR = 0x0000; // Clear counter
//
// Set Compare values
//
EPwm2Regs.CMPA.bit.CMPA = EPWM2_CMPA; // Set compare A value
EPwm2Regs.CMPB.bit.CMPB = EPWM2_CMPB; // Set Compare B value
//
// Setup counter mode
//
EPwm2Regs.TBCTL.bit.CTRMODE = TB_COUNT_UPDOWN; // Count up and down
EPwm2Regs.TBCTL.bit.PHSEN = TB_ENABLE; // Enable phase loading
EPwm2Regs.TBCTL.bit.PHSDIR = 1;
EPwm2Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1; // Clock ratio to SYSCLKOUT
EPwm2Regs.TBCTL.bit.CLKDIV = TB_DIV1;
//
// Setup shadowing
//
EPwm2Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW;
EPwm2Regs.CMPCTL.bit.SHDWBMODE = CC_SHADOW;
EPwm2Regs.CMPCTL.bit.LOADAMODE = CC_CTR_ZERO; // Load on Zero
EPwm2Regs.CMPCTL.bit.LOADBMODE = CC_CTR_ZERO;
//
// Set actions
//
EPwm2Regs.AQCTLA.bit.CAD = AQ_SET; // Set PWM2A on event A, up
// count
EPwm2Regs.AQCTLA.bit.CBD = AQ_CLEAR; // Clear PWM2A on event B, down
// count
// Active Low PWMs - Setup Deadband
//
EPwm2Regs.DBCTL.bit.OUT_MODE = DBB_ENABLE;
EPwm2Regs.DBCTL.bit.POLSEL = DB_ACTV_HI;
EPwm2Regs.DBCTL.bit.IN_MODE = DBA_ALL;
EPwm2Regs.DBRED.bit.DBRED = 0;
EPwm2Regs.DBFED.bit.DBFED = 0;
//
// Interrupt where we will change the Compare Values
//
EPwm2Regs.ETSEL.bit.INTSEL = ET_CTR_ZERO; // Select INT on Zero event
EPwm2Regs.ETSEL.bit.INTEN = 1; // Enable INT
EPwm2Regs.ETPS.bit.INTPRD = ET_3RD; // Generate INT on 3rd event
//
}
void ShutEPWM(void)
{
EALLOW;
EPwm1Regs.TZFRC.bit.OST = 1; // Force a one-shot trip event and sets ost bit
EPwm1Regs.TZCTL.bit.TZA = 2; // Force PWM to low level
EPwm1Regs.TZCTL.bit.TZB = 2; // Force PWM to low level
EPwm2Regs.TZFRC.bit.OST = 1; // Force a one-shot trip event and sets ost bit
EPwm2Regs.TZCTL.bit.TZA = 2; // Force PWM to low level
EPwm2Regs.TZCTL.bit.TZB = 2; // Force PWM to low level
EDIS;
}
void EnablePWM(void)
{
EALLOW;
EPwm1Regs.TZCLR.bit.OST = 1;
EPwm2Regs.TZCLR.bit.OST = 1;
EDIS;
}
//
// InitEPwm3Example - Initialize EPWM3 configuration
//
//
// End of file
//