This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
when trying External mode in MATLAB Simulink for TMDSCNCD28379D for CPU2 (Boot from Flash), I am already running a different application on CPU1 (Boot from Flash), I am getting an error saying "program will not fit into available memory"
<Linking> warning: build attribute vendor section TI missing in "C:/ProgramData/MATLAB/SupportPackages/R2018a/toolbox/target/supportpackages /tic2000/rtlib/IQmath_fpu32.lib<IQ10div.obj>": compatibility cannot be determined warning: build attribute vendor section TI missing in "C:/ProgramData/MATLAB/SupportPackages/R2018a/toolbox/target/supportpackages /tic2000/rtlib/IQmath_fpu32.lib<IQmathTables.obj>": compatibility cannot be determined "C:/ProgramData/MATLAB/SupportPackages/R2018a/toolbox/target/supportpackages/tic2000/src/c28377D.cmd", line 131: error: program will not fit into available memory. run placement with alignment/blocking fails for section ".ebss" size 0x8e7 page 1. Available memory ranges: RAMLS_DATA size: 0x2000 unused: 0x0 max hole: 0x0 RAMD1 size: 0x800 unused: 0x0 max hole: 0x0 error: errors encountered during linking; "../Inverter_003.out" not built >> Compilation failure gmake: *** [../Inverter_003.out] Error 1
The main part says:
RAMLS_DATA size: 0x2000 unused: 0x0 max hole: 0x0
RAMD1 size: 0x800 unused: 0x0 max hole: 0x0
This reply advises going into the Linker file and adding more sections to the heap area.
When I go to the Linker file C:\ProgramData\MATLAB\SupportPackages\R2018a\toolbox\target\supportpackages\tic2000\src\c28377D.cmd
Q1. I do not see .sysmem, only .esysmem. Is this a problem?
.esysmem : > RAMLS_DATA, PAGE = 1
Q2. There is only #ifdef CPU1 for CPU1 and not CPU2. Is this a problem?
Q3. I do not see available memory to add as OR ("|") in the linker file, only RAMLS_DATA. Should I modify RAMLS_DATA? Full Linker file is sjown below
#ifdef CLA_BLOCK_INCLUDED // Define a size for the CLA scratchpad area that will be used // by the CLA compiler for local symbols and temps // Also force references to the special symbols that mark the // scratchpad are. CLA_SCRATCHPAD_SIZE = 0x100; --undef_sym=__cla_scratchpad_end --undef_sym=__cla_scratchpad_start #endif //CLA_BLOCK_INCLUDED MEMORY { PAGE 0 : /* BEGIN is used for the "boot to SARAM" bootloader mode */ BEGIN : origin = 0x000000, length = 0x000002 BEGIN_FLASH : origin = 0x080000, length = 0x000002 #ifdef CPU1 RAMM0 : origin = 0x000122, length = 0x0002DE #else RAMM0 : origin = 0x000080, length = 0x000380 #endif RAMD0 : origin = 0x00B000, length = 0x000800 #ifdef CLA_BLOCK_INCLUDED RAMLS_PROG : origin = 0x00A000, length = 0x000800 RAMLS_CLA_PROG : origin = 0x00A800, length = 0x000800 #else RAMLS_PROG : origin = 0x009000, length = 0x002000 #endif //CLA_BLOCK_INCLUDED #ifdef CPU1 #if BOOT_FROM_FLASH RAMGS_PROG : origin = 0x017000, length = 0x001000 #else RAMGS_PROG : origin = 0x014000, length = 0x004000 #endif #endif RESET : origin = 0x3FFFC0, length = 0x000002 /* Flash sectors */ FLASHA_N : origin = 0x080002, length = 0x03FFFE /* on-chip Flash */ PAGE 1 : #ifdef CPU1 BOOT_RSVD : origin = 0x000002, length = 0x000120 /* Part of M0, BOOT rom will use this for stack */ #else BOOT_RSVD : origin = 0x000002, length = 0x00007E /* Part of M0, BOOT rom will use this for stack */ #endif RAMM1 : origin = 0x000400, length = 0x000400 /* on-chip RAM block M1 */ RAMD1 : origin = 0x00B800, length = 0x000800 #ifdef CLA_BLOCK_INCLUDED RAMLS_CLA_DATA : origin = 0x008000, length = 0x001000 RAMLS_DATA : origin = 0x009000, length = 0x002000 #else RAMLS_DATA : origin = 0x008000, length = 0x002000 #endif //CLA_BLOCK_INCLUDED #ifdef CPU1 #if BOOT_FROM_FLASH RAMGS_DATA : origin = 0x00E000, length = 0x00B000 #else RAMGS_DATA : origin = 0x00E000, length = 0x008000 #endif #endif RAMGS_IPCBuffCPU1 : origin = 0x00C000, length = 0x001000 RAMGS_IPCBuffCPU2 : origin = 0x00D000, length = 0x001000 CLA1_MSGRAMLOW : origin = 0x001480, length = 0x000080 CLA1_MSGRAMHIGH : origin = 0x001500, length = 0x000080 CPU2TOCPU1RAM : origin = 0x03F800, length = 0x000400 CPU1TOCPU2RAM : origin = 0x03FC00, length = 0x000400 } SECTIONS { #if BOOT_FROM_FLASH /* Allocate program areas: */ .cinit : > FLASHA_N PAGE = 0, ALIGN(4) .pinit : > FLASHA_N, PAGE = 0, ALIGN(4) .text : > FLASHA_N PAGE = 0, ALIGN(4) codestart : > BEGIN_FLASH PAGE = 0, ALIGN(4) ramfuncs : LOAD = FLASHA_N, RUN = RAMLS_PROG, LOAD_START(_RamfuncsLoadStart), LOAD_SIZE(_RamfuncsLoadSize), LOAD_END(_RamfuncsLoadEnd), RUN_START(_RamfuncsRunStart), RUN_SIZE(_RamfuncsRunSize), RUN_END(_RamfuncsRunEnd), PAGE = 0, ALIGN(4) /* Initalized sections go in Flash */ .econst : > FLASHA_N PAGE = 0, ALIGN(4) .switch : > FLASHA_N PAGE = 0, ALIGN(4) /* Allocate IQmath areas: */ IQmath : > FLASHA_N, PAGE = 0, ALIGN(4) /* Math Code */ IQmathTables : > FLASHA_N, PAGE = 0, ALIGN(4) #ifdef CLA_BLOCK_INCLUDED /* CLA specific sections */ Cla1Prog : LOAD = FLASHA_N, RUN = RAMLS_CLA_PROG, LOAD_START(_Cla1funcsLoadStart), LOAD_END(_Cla1funcsLoadEnd), RUN_START(_Cla1funcsRunStart), LOAD_SIZE(_Cla1funcsLoadSize), PAGE = 0, ALIGN(4) #endif //CLA_BLOCK_INCLUDED #else codestart : > BEGIN, PAGE = 0 ramfuncs : > RAMM0 PAGE = 0 #ifdef CPU1 .text : >>RAMM0 | RAMD0 | RAMLS_PROG | RAMGS_PROG, PAGE = 0 #else .text : >>RAMM0 | RAMD0 | RAMLS_PROG, PAGE = 0 #endif .cinit : > RAMM0 | RAMD0 | RAMLS_PROG | RAMGS_PROG, PAGE = 0 .pinit : > RAMM0, PAGE = 0 .switch : > RAMM0, PAGE = 0 .econst : > RAMLS_DATA, PAGE = 1 /* Allocate IQ math areas: */ IQmath : > RAMLS_PROG, PAGE = 0 /* Math Code */ IQmathTables : > RAMLS_PROG, PAGE = 0 #ifdef CLA_BLOCK_INCLUDED /* CLA specific sections */ Cla1Prog : > RAMLS_CLA_PROG, PAGE=0 #endif //CLA_BLOCK_INCLUDED #endif .stack : > RAMM1, PAGE = 1 #ifdef CPU1 .ebss : >> RAMLS_DATA| RAMD1 | RAMGS_DATA , PAGE = 1 #else .ebss : >> RAMLS_DATA| RAMD1, PAGE = 1 #endif .reset : > RESET, PAGE = 0, TYPE = DSECT /* not used, */ .esysmem : > RAMLS_DATA, PAGE = 1 #ifdef CLA_BLOCK_INCLUDED /* CLA C compiler sections */ // // Must be allocated to memory the CLA has write access to // Cla1DataRam0 : > RAMLS_CLA_DATA, PAGE=1 Cla1ToCpuMsgRAM : > CLA1_MSGRAMLOW, PAGE = 1 CpuToCla1MsgRAM : > CLA1_MSGRAMHIGH, PAGE = 1 CLAscratch : { *.obj(CLAscratch) . += CLA_SCRATCHPAD_SIZE; *.obj(CLAscratch_end) } > RAMLS_CLA_DATA, PAGE = 1 .scratchpad : > RAMLS_CLA_DATA, PAGE = 1 .bss_cla : > RAMLS_CLA_DATA, PAGE = 1 .const_cla : LOAD = FLASHA_N, RUN = RAMLS_CLA_DATA, RUN_START(_Cla1ConstRunStart), LOAD_START(_Cla1ConstLoadStart), LOAD_SIZE(_Cla1ConstLoadSize), PAGE = 1 #endif //CLA_BLOCK_INCLUDED #ifdef CPU1 /* The following section definitions are required when using the IPC API Drivers */ GROUP : > CPU1TOCPU2RAM, PAGE = 1 { PUTBUFFER PUTWRITEIDX GETREADIDX WRITEFLAG1CPU1 WRITEFLAG2CPU1 READFLAG1CPU1 READFLAG2CPU1 } GROUP : > CPU2TOCPU1RAM, PAGE = 1 { GETBUFFER : TYPE = DSECT GETWRITEIDX : TYPE = DSECT PUTREADIDX : TYPE = DSECT WRITEFLAG1CPU2: TYPE = DSECT WRITEFLAG2CPU2: TYPE = DSECT READFLAG1CPU2: TYPE = DSECT READFLAG2CPU2: TYPE = DSECT } #else /* The following section definitions are required when using the IPC API Drivers */ GROUP : > CPU2TOCPU1RAM, PAGE = 1 { PUTBUFFER PUTWRITEIDX GETREADIDX WRITEFLAG1CPU2 WRITEFLAG2CPU2 READFLAG1CPU2 READFLAG2CPU2 } GROUP : > CPU1TOCPU2RAM, PAGE = 1 { GETBUFFER : TYPE = DSECT GETWRITEIDX : TYPE = DSECT PUTREADIDX : TYPE = DSECT WRITEFLAG1CPU1: TYPE = DSECT WRITEFLAG2CPU1: TYPE = DSECT READFLAG1CPU1 : TYPE = DSECT READFLAG2CPU1 : TYPE = DSECT } #endif GROUP : > RAMGS_IPCBuffCPU1, PAGE = 1 { CPU1TOCPU2GSRAM } GROUP : > RAMGS_IPCBuffCPU2, PAGE = 1 { CPU2TOCPU1GSRAM } } /* //=========================================================================== // End of file. //=========================================================================== */
I asked a similar question several months ago as I was having the same error ("program will not fit into available memory") and I assumed increasing the heap size from the MATLAB Simulink will solve the problem. It did, temporarily, but now I am still having the same issue.
Hi,
Q1. I do not see .sysmem, only .esysmem. Is this a problem?
.esysmem : > RAMLS_DATA, PAGE = 1
Looks like you are using COFF format, so .esysmem is equivalent section.
Q2. There is only #ifdef CPU1 for CPU1 and not CPU2. Is this a problem?
This should not be any issue. If not CPU1 block for CPU2.
I do not see available memory to add as OR ("|") in the linker file, only RAMLS_DATA. Should I modify RAMLS_DATA?
Do you have CLA_BLOCK_INCLUDED ? If not then you may be able include RAMLS_DATA little bit.
is this linker file came with Simulink project or you created for your project?
Hi Santosh,
the linker file came with the Simulink Support Package for C2000 installation from the MATLAB website. I do not see F28379D (processor which I am using) so the 'closest' is c28377D.cmd. In the Simulink I have set the linker command file path to that file. Is there a specific linker file for F28379D available to download?
There is a CLA_BLOCK_INCLUDED, line #136 in my first message showing the full linker file.
Line #50 and #52 in linker file say
RAMLS_DATA : origin = 0x009000, length = 0x002000 (#50)
RAMLS_DATA : origin = 0x008000, length = 0x002000 (#52)
would a solution be to increase the lenght? Can this be done? To how much?
For the F28377D (which is similar to the F28379D processor) it says there is "128KB of GSx RAMs (16 blocks of 8KB)". Now sure how to convert length 0x002000 to KB and check if I still have a space left.
MATLAB Simulink report says
RAMLS_DATA size: 0x2000 unused: 0x0
meaning, all 2000 is used.
Hi Santosh,
New update. When I load the application (e.g. Machine Side App) on CPU1 in External mode for testing and parameter tuning and another already tested (e.g. Network Side App) on the CPU2 (not in External mode), I am not getting an error.
But, I get a different problem. I do not see any change in the application: my ADCs are zero although there is a 1.5 Vdc input (offset for AC signals to accomodate unipolar ADC input) and GPIO toggle signal I have to verify the sample time (10 kHz) is always HIGH.
I used F28335 before and was able to run a similar code (Network and Machine App on one CPU -- F28335 has only one CPU). F28379D has two CPUs and more memory.
Would increasing RAM length help and can I add more RAM locations? Am I on the right track?
When I do OR between all RAMs, I get 0x002200 + 0x000800 + 0x004000 which is 0x007000 bites, compared to 1024 KB of memory F28739D has... am I correctly adding all this?
.esysmem : > RAMLS_DATA | RAMD1 | RAMGS_DATA
No, no, Sorry if I added a level of confusion here. They are my bespoke Simulink applications to control network (loaded onto CPU1) and machine (loaded onto CPU2) converter. Each has an ADC section, scaling and filtering, dual-loop control and PWM blocks.
I have modified the ADC block slightly and changed the acquisition window and it is ok now. I am slowly re-building the application code bit by bit from scratch, compiling and loading the code as I go, checking for overruns, etc., and so far everything is ok.
Btw. is there somewhere a Linker file specifically for F28379D with all RAM properly assigned?
Mike,
Sorry for the delay on our side, alot of us were out last week, and I'm following up on Santosh's threads.
In terms of a superset .cmd file I'd start here C:\ti\c2000\C2000Ware_4_00_00_00\device_support\f2837xd\common\cmd\2837xD_FLASH_lnk_cpu1.cmd
Based on the earlier posts, I think the linker error may persist even if you join multiple RAMs with the "|" operator. This can happen if there is a function that crosses defined boundaries of the defined RAMs, and why the linker will report a size of 0.
If this is still the case, you will need to manually combine RAMs with longer length(I think you mentioned this earlier). You could do this to get the contiguous block to be as big as needed for a particular section.
Let me know if this is on the right track or there's some more digging I need to do.
Best,
Matthew