Part Number: TMS320F28379D
Other Parts Discussed in Thread: C2000WARE
Dear team,
I have a use-case where I need to have a single image with CPU1 and CPU2 together, meaning there should not be two separate images for both cores, but a final single image. For this, I have been able to generate the .hex output of CPU2 image (as an array) which I have stored within build for CPU1.
I want to load the CPU2 image from CPU1 post CPU1 is booted-up, which I feel is possible using boot ROM via IPCs supported by CPU2 boot ROM, but not sure on how that should be executed. For now, I'm calling IPCLite functions used in demo projects for IPC, but CPU1 is not able to get the ACK from boot ROM for any of the operations (be it then 16-bit read/write operation or 32-bit/write operation).
Please guide on how to get ACK from CPU2's boot-ROM.
Regards,
Sumit Panse