Part Number: TMS320F28P650DK
Other Parts Discussed in Thread: UNIFLASH
Tool/software:
Hi champs,
I am asking this for our customer.
Can the user use CPU1 to program a combined image for both CPU1 and CPU2 in the production line?
For example,
CPU1 has a CPU1.out running on flash bank0/1/2.
CPU2 has a CPU2.out running on flash bank3/4.
The user converts each .out to .hex and combined them into a combined image ALL.hex.
Then, the user makes an SCI programmer using TI SCI ROM bootloader/SCI boot mode pins with the kernel using CPU1 to program ALL.hex on flash bank 0/1/2/3/4 once.
That is, in the kernel code, CPU1 configures all flash bank0/1/2/3/4 to CPU1 for programming.
On normal standalone mode, CPU1 configures bank0/1/2 to CPU1 and bank3/4 to CPU2 and run each .out accordingly.
Do you think it works?