Part Number: TMS320F28388D
Dear Experts,
my customer is facing an issue when running the "mcan_ex9_transmit" example and try to debug the application using breakpoints or pausing the execution. They are using an external CAN receiver.
After loading the code and running the example, my customer would like to debug the code and enter breakpoints.
He noticed, that after inserting a breakpoint, stopping at the breakpoint and then let the code run again, the CAN communication is not working anymore. So something breaks, when entering CPU debug state.
Is there a way to debug the application without breaking the MCAN communication or without the need to PoR the complete device?
Could you please let me know, if there is a way to reset the MCAN controller/communication only and will this be sufficient to restart proper Tx/Rx of MCAN packets?
Thanks and best regards,
Gregor