Part Number: TMS320F280049
Other Parts Discussed in Thread: UNIFLASH
Dear Champs,
I am asking this for a customer.
They use a bootloader/kernel project, an application project with DCSM/passwords generated by the DCSM GUI.
Because there are two CCS projects, there are two corresponding output files (.out).
Now, they want to program these two .out images once in the production line.
That is, they wonder how they can use one image to program these by the operator just for one time.
Do you have any suggestion how they can do this?
Does it make sense they program F280049 with these two projects (.out files) separately on the engineer's side first and then use Uniflash to unlock F280049 and read out all flash and OTP contents and then save it into a new .out file as an image?
Wayne Huang