This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Currently the we are hitting a memory limit of the mentioned uC. To overcome this issue some code fragments are stored in an external eeprom. For ramfuncs and the cla segments this is relatively easy and works fine. The modification to the linker file etc. could be made within a few hours. Now comes the challenging part: We have large binary like structures that are currently stored in flash and only used once in a while. The idea is to store them in the external memory as well and only load them sequentely when needed. The idea was to create a dummy section in the linker file and command the linker to put the structure in the dummy section. Once linking has finished i want to create a hex file of the afore mentioned section using the HEX2000 utility. Unfortunately the utility tells me that this would fall in unconfigured memory and therefore is going to be skipped. Any ideas how to "force" the utility to just write this section to a hex file? The linker itself however has no problems with linking the external sections, problems start when i try to load or process the linked binary any further.
Thanks in advance Tobias F.
Please describe this part in more detail ...
We have large binary like structures that are currently stored in flash and only used once in a while. The idea is to store them in the external memory as well and only load them sequentely when needed. The idea was to create a dummy section in the linker file and command the linker to put the structure in the dummy section.
Please attach the linker command file to your next post. So that the forum will accept it, add the file extension .txt to it.
Thanks and regards,
-George
/* //########################################################################### // // FILE: F28069.cmd // // TITLE: Linker Command File For F28069 Device // //########################################################################### // $TI Release: F2806x C/C++ Header Files and Peripheral Examples V150 $ // $Release Date: June 16, 2015 $ // $Copyright: Copyright (C) 2011-2015 Texas Instruments Incorporated - // http://www.ti.com/ ALL RIGHTS RESERVED $ //########################################################################### */ /* ====================================================== // For Code Composer Studio V2.2 and later // --------------------------------------- // In addition to this memory linker command file, // add the header linker command file directly to the project. // The header linker command file is required to link the // peripheral structures to the proper locations within // the memory map. // // The header linker files are found in <base>\F2806x_headers\cmd // // For BIOS applications add: F2806x_Headers_BIOS.cmd // For nonBIOS applications add: F2806x_Headers_nonBIOS.cmd ========================================================= */ /* ====================================================== // For Code Composer Studio prior to V2.2 // -------------------------------------- // 1) Use one of the following -l statements to include the // header linker command file in the project. The header linker // file is required to link the peripheral structures to the proper // locations within the memory map */ /* Uncomment this line to include file only for non-BIOS applications */ /* -l F2806x_Headers_nonBIOS.cmd */ /* Uncomment this line to include file only for BIOS applications */ /* -l F2806x_Headers_BIOS.cmd */ /* 2) In your project add the path to <base>\F2806x_headers\cmd to the library search path under project->build options, linker tab, library search path (-i). /*========================================================= */ /* Define the memory block start/length for the F2806x PAGE 0 will be used to organize program sections PAGE 1 will be used to organize data sections Notes: Memory blocks on F28069 are uniform (ie same physical memory) in both PAGE 0 and PAGE 1. That is the same memory region should not be defined for both PAGE 0 and PAGE 1. Doing so will result in corruption of program and/or data. Contiguous SARAM memory blocks can be combined if required to create a larger memory block. */ //Cla1Prog_Start = Cla1funcsRunStart; -heap 10 -stack 944 // Define a size for the CLA scratchpad area that will be used // by the CLA compiler for local symbols and temps // Also force references to the special symbols that mark the // scratchpad are. CLA_SCRATCHPAD_SIZE = 0x200; --undef_sym=__cla_scratchpad_end --undef_sym=__cla_scratchpad_start MEMORY { PAGE 0 : /* Program Memory */ /* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE1 for data allocation */ OTP : origin = 0x3D7800, length = 0x0003F6 /* on-chip OTP | keep distance to OTP_KEY and OTP_BMODE */ RAML3 : origin = 0x009000, length = 0x001000 /* Cla Programm Ram */ //RAML5 : origin = 0x00C000, length = 0x002000 // ramfuncs TODO move ramfuncs to L7 and place taskdata / heap here RAML7 : origin = 0x010000, length = 0x002000 /* on-chip RAM block L7 */ FLASHH : origin = 0x3D8000, length = 0x004000 /* on-chip FLASH*/ FLASHG : origin = 0x3DC000, length = 0x004000 /* on-chip FLASH */ FLASHEF : origin = 0x3E0000, length = 0x008000 /* fusion of flash E and Flash F*/ FLASHD : origin = 0x3E8000, length = 0x004000 /* on-chip FLASH */ FLASHC : origin = 0x3EC000, length = 0x004000 /* on-chip FLASH */ FLASHB : origin = 0x3F0000, length = 0x004000 /* on-chip FLASH */ FLASHA : origin = 0x3F4000, length = 0x003F80 /* on-chip FLASH */ CSM_RSVD : origin = 0x3F7F80, length = 0x000076 /* Part of FLASHA. Program with all 0x0000 when CSM is in use. */ BEGIN : origin = 0x3F7FF6, length = 0x000002 /* Part of FLASHA. Used for "boot to Flash" bootloader mode. */ CSM_PWL_P0 : origin = 0x3F7FF8, length = 0x000008 /* Part of FLASHA. CSM password locations in FLASHA */ // LUT in Boot Rom FPUTABLES : origin = 0x3FD860, length = 0x0006A0 /* FPU Tables in Boot ROM */ IQTABLES : origin = 0x3FDF00, length = 0x000B50 /* IQ Math Tables in Boot ROM */ IQTABLES2 : origin = 0x3FEA50, length = 0x00008C /* IQ Math Tables in Boot ROM */ IQTABLES3 : origin = 0x3FEADC, length = 0x0000AA /* IQ Math Tables in Boot ROM */ ROM : origin = 0x3FF3B0, length = 0x000C10 /* Boot ROM */ RESET : origin = 0x3FFFC0, length = 0x000002 /* part of boot ROM */ VECTORS : origin = 0x3FFFC2, length = 0x00003E /* part of boot ROM */ EXT_MEM : origin = 0x000, length = 0x7530 /* eeprom workaround*/ PAGE 1 : /* Data Memory */ /* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE0 for program allocation */ /* Registers remain on PAGE1 */ BOOT_RSVD : origin = 0x000000, length = 0x000050 /* Part of M0, BOOT rom will use this for stack */ RAMM0 : origin = 0x000050, length = 0x0003B0 // used as stack RAMM1 : origin = 0x000400, length = 0x000400 // used as c stack RAML0 : origin = 0x008000, length = 0x000800 // used for rtos task stack RAML4 : origin = 0x00A000, length = 0x002000 // dito and as heap extension RAML5 : origin = 0x00C000, length = 0x002000 // dito RAML6 : origin = 0x00E000, length = 0x002000 // used as heap highest stack pointer range !!! //RAML7 : origin = 0x010000, length = 0x002000 /* on-chip RAM block L7 */ RAML8 : origin = 0x012000, length = 0x002000 /* on-chip RAM block L8 */ USB_RAM : origin = 0x040000, length = 0x000800 /* USB RAM */ CLARAM0 : origin = 0x008800, length = 0x000400 /* Replaces RAML1 */ CLARAM1 : origin = 0x008C00, length = 0x000400 CLA1_MSGRAMLOW : origin = 0x001480, length = 0x000080 CLA1_MSGRAMHIGH : origin = 0x001500, length = 0x000080 } /* Allocate sections to memory blocks. Note: codestart user defined section in DSP28_CodeStartBranch.asm used to redirect code execution when booting to flash ramfuncs user defined section to store functions that will be copied from Flash into RAM */ SECTIONS { /* Allocate program areas: */ .cinit : > FLASHEF | FLASHH, PAGE = 0, crc_table(FlashCrc) .text : >> FLASHA | FLASHB | FLASHC | FLASHD | FLASHG | FLASHEF, PAGE = 0, crc_table(FlashCrc) codestart : > BEGIN, PAGE = 0 /* .TI.ramfunc : LOAD = FLASHH, RUN = RAML5, LOAD_START(TiRamfuncsLoadStart), LOAD_END(TiRamfuncsLoadEnd), RUN_START(TiRamfuncsRunStart), LOAD_SIZE(TiRamfuncsLoadSize), crc_table(RamfuncsCrc) // also add to Flash Crc Table */ .TI.ramfunc : > RAML7, RUN_START(TiRamfuncsRunStart), RUN_SIZE(TiRamfuncsLoadSize), PAGE = 0, crc_table(RamfuncsCrc) csmpasswds : > CSM_PWL_P0, PAGE = 0 csm_rsvd : > CSM_RSVD, PAGE = 0 /* Allocate uninitalized data sections: */ .stack : > RAMM0, PAGE = 1 // stack .ebss : > RAML8, PAGE = 1 // generic ram data .bss : >> RAML8 | USB_RAM,PAGE = 1 // generic ram data .esysmem : > RAML8, PAGE = 1 // heap .sysmem : > RAML8, PAGE = 1 /* Initalized sections to go in Flash */ /* For SDFlash to program these, they must be allocated to page 0 */ .const : >> FLASHG | FLASHEF | FLASHH, PAGE = 0, crc_table(FlashCrc) .init_array : > FLASHEF, PAGE = 0, crc_table(FlashCrc) .switch : > FLASHEF, PAGE = 0, crc_table(FlashCrc) .data : > RAML8, PAGE = 1 /* Allocate IQ math areas: */ IQmath : > FLASHA, PAGE = 0 IQmathTables : > IQTABLES, PAGE = 0, TYPE = NOLOAD /* Allocate FPU math areas: */ FPUmathTables : > FPUTABLES, PAGE = 0, TYPE = NOLOAD DMARAML5 : > RAML6, PAGE = 1 DMARAML6 : > RAML6, PAGE = 1 //DMARAML7 : > RAML7, PAGE = 1 DMARAML8 : > RAML8, PAGE = 1 /* Cla Stuff */ .scratchpad : > CLARAM0, PAGE = 1 .bss_cla : > CLARAM0, PAGE = 1 .const_cla : > CLARAM0, PAGE = 1 Cla1ToCpuMsgRAM : > CLA1_MSGRAMLOW, PAGE = 1 CpuToCla1MsgRAM : > CLA1_MSGRAMHIGH, PAGE = 1 /* Cla1Prog : LOAD = FLASHH, PAGE = 0, RUN = RAML3, LOAD_START(Cla1funcsLoadStart), LOAD_END(Cla1funcsLoadEnd), RUN_START(Cla1funcsRunStart), LOAD_SIZE(Cla1funcsLoadSize), crc_table(ClaCrc) */ Cla1Prog : > RAML3, PAGE = 0, RUN_START(Cla1ProgRunStart), RUN_SIZE(Cla1ProgRunSize), crc_table(ClaCrc) Cla1DataRam0 : > CLARAM0, PAGE = 1 Cla1DataRam1 : > CLARAM1, PAGE = 1 /* CLA1mathTables : LOAD = EEPROM, PAGE = 0, RUN = CLARAM1, PAGE = 1, LOAD_START(Cla1mathTablesLoadStart), LOAD_END(Cla1mathTablesLoadEnd), LOAD_SIZE(Cla1mathTablesLoadSize), RUN_START(Cla1mathTablesRunStart), crc_table(ClaCrc) */ CLA1mathTables : > CLARAM1, PAGE = 1, RUN_START(Cla1mathTablesRunStart), RUN_SIZE(Cla1mathTablesLoadSize), crc_table(ClaCrc) CLAscratch : { *.obj(CLAscratch) . += CLA_SCRATCHPAD_SIZE; *.obj(CLAscratch_end) } > CLARAM0, PAGE = 1 /* used for rtos heap */ rtos_heap : > RAML6 PAGE = 1 //rtos_heap_ext : > RAML5 PAGE = 0 rtos_heap_m1 : > RAMM1 PAGE = 1 (HIGH) rtos_heap_l4 : > RAML4 PAGE = 1 /* Data Section for Task Stack Memory */ task_data : >> RAML0 | RAMM0 | RAML4, PAGE = 1 /* Data Section in Flash for Settings etc */ .cio : > RAML8, PAGE = 1 .TI.crctab : > FLASHEF | FLASHH, PAGE = 0 .clean : > FLASHD, PAGE = 0 .c28xabi.extab : > FLASHEF, PAGE = 0 // crc tables maybe work in the future until then we have to hope for the best .c28xabi.exidx : > FLASHH, PAGE = 0 OTP_ROM : > FLASHEF, PAGE = 0 // someday this is copied into otp, maybe /*config and cli elements in external eeprom*/ .config : {*Config*.* (.const)} > FLASHEF, PAGE = 0 .cli_scmd : {CliCmdDeflated.obj (.const)} > EXT_MEM, PAGE = 0, RUN_SIZE(CliScmdSize) /* Flash28_API: { -l flash_api_f2806x_eabi.lib(.text) -l flash_api_f2806x_eabi.lib(.const) -l flash_api_f2806x_eabi.lib(.econst) } LOAD = FLASHF, RUN = RAML5, LOAD_START(Flash28_API_LoadStart), LOAD_SIZE(Flash28_API_LoadSize), LOAD_END(Flash28_API_LoadEnd), RUN_START(Flash28_API_RunStart), PAGE = 0, crc_table(FlashCrc) */ /* Uncomment the section below if calling the IQNexp() or IQexp() functions from the IQMath.lib library in order to utilize the relevant IQ Math table in Boot ROM (This saves space and Boot ROM is 1 wait-state). If this section is not uncommented, IQmathTables2 will be loaded into other memory (SARAM, Flash, etc.) and will take up space, but 0 wait-state is possible. */ /* IQmathTables2 : > IQTABLES2, PAGE = 0, TYPE = NOLOAD { IQmath.lib<IQNexpTable.obj> (IQmathTablesRam) } */ /* Uncomment the section below if calling the IQNasin() or IQasin() functions from the IQMath.lib library in order to utilize the relevant IQ Math table in Boot ROM (This saves space and Boot ROM is 1 wait-state). If this section is not uncommented, IQmathTables2 will be loaded into other memory (SARAM, Flash, etc.) and will take up space, but 0 wait-state is possible. */ /* IQmathTables3 : > IQTABLES3, PAGE = 0, TYPE = NOLOAD { IQmath.lib<IQNasinTable.obj> (IQmathTablesRam) } */ /* .reset is a standard section used by the compiler. It contains the */ /* the address of the start of _c_int00 for C Code. /* /* When using the boot ROM this section and the CPU vector */ /* table is not needed. Thus the default type is set here to */ /* DSECT */ .reset : > RESET, PAGE = 0, TYPE = DSECT vectors : > VECTORS, PAGE = 0, TYPE = DSECT } /* //=========================================================================== // End of file. //=========================================================================== */
currently the .cli_scmd section is interesting, as can be seen the section is linked to external memory which start at 0. Usually this is no problem, except that sometimes a null pointer is still valid, but this isnt an issue here
I suspect the .cli_scmd output section does not work as you intend. Let's review how it is specified ...
.cli_scmd : {CliCmdDeflated.obj (.const)} > EXT_MEM, PAGE = 0, RUN_SIZE(CliScmdSize)
This says to create an output section named .cli_scmd. It is made up of one input section, the .const section from CliCmdDeflated.obj. It is allocated to an address in the memory range EXT_MEM.
Therefore, the entire program assumes that this output section is always located at this address in EXT_MEM. Is that the case? If so, why is the symbol CliScmdSize created? What is it used for?
Thanks and regards,
-George
Hello George,
Your assumptions are correct so far, as the external memory is read only any external reference are loaded during runtime through a custom handler. The size of the section is used to identify where this particular section starts in the generated blob. Currently there are multiple section in the external eeprom and therefore i have to calculate their start address (with ext_mem) and the size. The ramfuncs and cla prog and math tables follow the same scheme.
The problem is located in the hex utility which returns an error if i want to create a hex file for only the .cli_scmd section as mentioned above.
Thanks in advance Tobias Faschingbauer
i want to create a hex file for only the .cli_scmd section
To limit the output of the hex utility to only one section, create a hex command file that contains a SECTIONS directive. For details, please search the C28x assembly tools manual for the chapter titled Hex Conversion Utility Description. From there, click on the sub-chapter titled The SECTIONS Directive.
Thanks and regards,
-George
I was able to resolve the issue by now, the section directive alone is not sufficient, i had to use a rom directive as well. There i can specify the external memory and now it works like a charm.
Thanks for your time Tobias Faschingbauer