Other Parts Discussed in Thread: TMS320F280025C
I am working on C2000WARE-MOTORCONTROL-SDK. DC power supply of 220V is given to the Pfc and a JTAG(XDS110) which is connected to the Pfc from the system and the motor is also connected to the Pfc. After running the program and debugging there are no errors. After that I loaded the program to the Pfc and turned on the motor. Now I changed the rmp value the motor started running it worked upto1400rmp after that when I give the value 1500rmp It shows error then the Pfc and system disconnect and the motor stops running.
Is there any solution for this?