Part Number: TMS320F2812
Dear team:
My customer has some quesstions about SCI recive error.
1, When a receive error occurs in the SCI, if SW RESET is not performed, the RX ERROR bit will always be 1. At this time, if RXERRINTENA is enabled, the interrupt should be continuously entered. Why can't the interrupt be entered in the actual situation, even if the correct data is sent, the interrupt cannot be entered?
2, In the query mode, a receiving error occurs (for example, the receiving bus keeps low level), if the RX ERROR is not reset, can the data be received normally after the bus returns to normal?
Best regards