Other Parts Discussed in Thread: C2000WARE
I'm having some motor stability problems (salls on start stopping above 15krpm) with my custom code base after I upgraded to the SDK_3_03 and transferred to the standalone C:\ti\c2000\C2000Ware_MotorControl_SDK_3_03_00_00\libraries\observers\est_lib\lib\fast_flash_lib.lib
I have been trying to update to the latest SDK_4 and get a fresh copy of the "universal_motorcontrol_lab_f28002x" but before I got to this I can see there are lots of libs now and I can't find anything explaining which ones to use? as they seem to lock up on my custom project
C:\ti\c2000\C2000Ware_MotorControl_SDK_4_00_00_00\libraries\observers\est_lib\lib
fast_flash_lib.lib
fast_full_lib.lib
fast_pmsm_lib.lib
fast_simple_lib.lib
what are these for? and which one has different interfaces, which est.h do I use, and what #defines are needed?
#if defined(_FULL_FAST_LIB)
Cheers,
Alan