Part Number: SM320F28335-EP
Other Parts Discussed in Thread: C2000WARE, TEST2, UNIFLASH
Team,
Can you please help with the below?
More details (tools used, API version and error message) will be added soon.
The Flash is being written in two steps:
1) A custom bootloader is written to flash via the Lauterbach emulator
2) The custom bootloader burns the flash with the Final application using the Flash APIs
On the evaluation board both step 1 and 2 work accordingly.
But on the production board the step 2 fails. The Flash API return an error and the Flash cannot be recovered.
This happen on multiple boards of the 1st production batch.
Thanks in advance,
A.