Other Parts Discussed in Thread: C2000WARE
Does anyone know if it is possible to use the GPIO133/AUXCLKIN pin on the TMS320F28379s as a general purpose output? If so, do I need something different in my configuration to use it as an output? My code doesn't seem to let me control it as an output:-
GPIO_setPadConfig(EN_400V, GPIO_PIN_TYPE_STD); // Enable pullup on GPIO133
GPIO_writePin(EN_400V, 0); // Load output latch
GPIO_setPinConfig(GPIO_133_GPIO133); // GPIO133 = GPIO133 (Enable for 400V PSU)
GPIO_setDirectionMode(EN_400V, GPIO_DIR_MODE_OUT); // GPIO133 = output
Here, EN_400V is defined as 133
When I use the same code on GPIO132, I am able to configure it as an output and change its state like a normal GPIO
Thanks, Iain