This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
This is a question about the speed of cpu1 and cpu2 of the f28377d dual core.
If I only activate cpu1 of f28377d, one loop takes 1s.
But when I enable cpu1 and cpu2, cpu1 takes more than 5 seconds in one loop. (All interrupts of cpu2 were tested in the disabled state.)
The processing speed of cpu1 has been slowed down.
It seems to be a ccs configuration problem.
The attached picture is the edited screen.
Can you give me some advice?
Thak you.
Hi,
Is there any handshake mechanism between the cores?
Thanks & Regards,
Santosh