Hello,
I had a few questions about Figure 7-18 in the TMS320F28002x datasheet.
The figure shows the 20-pin JTAG header connection, and I had 4 questions:
1) what is open drain and where does it connect to?
2) does the 3.3V supply on pins 13 and 14 come from the MCU? If not, where does it come from?
3) are the GND pins connected to the GND of the MCU? If not, where do I ground them?
4) it says that TDI and TDO connections are optional for cJTAG. I am not sure if I will be using JTAG or cJTAG. Are there any advantages of using cJTAG over JTAG? Would I lose any functionalities if I choose to use cJTAG?
Thanks in advance!