This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28386S: lwip UDP - messages are not sent, only after received.

Part Number: TMS320F28386S

Hi,

I am testing tie sample project provided for the 28388 device.

I need to use several Sockets.

```

g_upcb1 = udp_new();
udp_bind(g_upcb, IP_ADDR_ANY, 2000);
udp_recv(g_upcb, &udp_rx_callback, (void*) 1);

g_upcb2 = udp_new();
udp_bind(g_upcb1, IP_ADDR_ANY, 3000);
udp_recv(g_upcb1, &udp_rx_callback, (void*) 2);

```

I need to receive a message from socket 1 and send a different message to socket 2.

I use 2 UDP terminals on my PC with different ports to test the application.

Port 2000 is the command port, and port 3000 is the slave port.

The test is to send from the computer a command from port 2000, have the CM send a message to the slave at port 3000.

The issue I see is that messages are not received on the PC at port 3000.

Only, after I send a message from port 3000 to the CM, than messages are received at port 3000.

It appear as if, the MC will not send out messages before receiving on a specific port.

Any ideas how to fix this behavior?

  • Givon, 

    Looking at the example for UDP, it expects a string 'START' to start sending the messages.  the boolen flag 'Connected_udp_28000' is set to true only when it receives this string and then invokes 'udp_send' to send the message. 

    You will have to update this logic to send out messages before receving the 'START" string.

    Best Regards

    Siddharth

  • Hi, 

    I have of course changed the logic.
    I understand this was not clear.

    Please see attached file I use for testing

    /*
     * Ethernet.c
     *
     *  Created on: 3 Nov 2022
     *      Author: Nir Givon
     */
    
    //###########################################################################
    //
    // TITLE:  lwIP based Ethernet Example.
    //
    // Example to demonstrate UDP socket (for daikin customer)
    // buf_rx,buf_tx are the watch variables which can be used or updated in the
    // main application based on the requirement.
    //
    // Test setup
    //
    // F2838x Control Card connected to a PC/laptop  on the Ethernet port.
    // PC/laptop runs the SocketTest/’Packet Sender’ software, configured for the IP Address and port . \
    // Keywords ‘START’ and ‘STOP’ are used to send and stop receiving messages respectively
    // Received data is stored in ‘buf_rx’ array and data to be transmitted is stored in ‘buf_tx’ array on CM core of F2838x device
    // Examples is Interrupt based with a callback function ‘udp_rx_callback’ which handles the received data from the SocketTest/Packet Sender software.
    //
    //###########################################################################
    // $TI Release: $
    // $Release Date: $
    // $Copyright:
    // Copyright (C) 2022 Texas Instruments Incorporated - http://www.ti.com
    //
    // Redistribution and use in source and binary forms, with or without
    // modification, are permitted provided that the following conditions
    // are met:
    //
    //   Redistributions of source code must retain the above copyright
    //   notice, this list of conditions and the following disclaimer.
    //
    //   Redistributions in binary form must reproduce the above copyright
    //   notice, this list of conditions and the following disclaimer in the
    //   documentation and/or other materials provided with the
    //   distribution.
    //
    //   Neither the name of Texas Instruments Incorporated nor the names of
    //   its contributors may be used to endorse or promote products derived
    //   from this software without specific prior written permission.
    //
    // THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
    // "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
    // LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
    // A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
    // OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
    // SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
    // LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
    // DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
    // THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
    // (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
    // OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
    // $
    //###########################################################################
    
    
    #include <string.h>
    
    #include "Ethernet.h"
    
    #include "inc/hw_ints.h"
    #include "inc/hw_memmap.h"
    #include "inc/hw_nvic.h"
    #include "inc/hw_types.h"
    #include "inc/hw_sysctl.h"
    #include "inc/hw_emac.h"
    
    #include "driverlib_cm/ethernet.h"
    #include "driverlib_cm/gpio.h"
    #include "driverlib_cm/interrupt.h"
    #include "driverlib_cm/flash.h"
    
    #include "driverlib_cm/sysctl.h"
    
    #include "utils/lwiplib.h"
    #include "board_drivers/pinout.h"
    
    
    #include "lwipopts.h"
    #include "ipc.h"
    
    
    #define PAYLOAD 1088
    
    volatile uint32_t msTime=0;
    
    
    volatile bool flag_TX_frame_UDP=true;
    
    
    #define MAKE_IP_ADDRESS(a0,a1,a2,a3) (((a0<<24) & 0xFF000000) | ((a1<<16) & 0x00FF0000) | ((a2<<8)  & 0x0000FF00) | (a3 & 0x000000FF) )
    
    bool Connected_udp_28000 = false;
    
    
    uint16_t cnt_Command_Pan = 0;
    uint16_t cnt_Command_Tilt = 0;
    uint16_t cnt_Command_Zoom = 0;
    
    uint16_t cnt_Command_Commands = 0;
    
    int sendTo1 = 0;
    bool sendTo2 = false;
    
    //
    // Defines
    //
    
    #define TEST_PASS          0x5555
    #define TEST_FAIL          0xAAAA
    
    //
    // Defines
    //
    #define PACKET_LENGTH 132
    
    struct udp_pcb *g_upcb_GUI;
    struct udp_pcb *g_upcb_Plots;
    struct udp_pcb *g_upcb_Decoder;
    
    
    
    u8_t buf_rx[PAYLOAD];
    u8_t buf_tx[PAYLOAD];
    char * buf_tx_start_msg = "Something to show UDP is working \n";
    uint32_t buf_tx_start_msg_count = 35;
    
    uint16_t cont_rx_udp = 0;
    
    struct pbuf *pbuf1_tx;
    
    
    //*****************************************************************************
    //
    //! \addtogroup master_example_list
    //! <h1>Ethernet with lwIP (enet_lwip)</h1>
    //!
    //! This example application demonstrates the operation of the F2838x
    //! microcontroller Ethernet controller using the lwIP TCP/IP Stack. Once
    //! programmed, the device sits endlessly waiting for ICMP ping requests. It
    //! has a static IP address. To ping the device, the sender has to be in the
    //! same network. The stack also supports ARP.
    //!
    //! For additional details on lwIP, refer to the lwIP web page at:
    //! http://savannah.nongnu.org/projects/lwip/
    //
    //*****************************************************************************
    
    // These are defined by the linker (see device linker command file)
    //extern uint16_t RamfuncsLoadStart;
    //extern uint16_t RamfuncsLoadSize;
    //extern uint16_t RamfuncsRunStart;
    //extern uint16_t RamfuncsLoadEnd;
    //extern uint16_t RamfuncsRunEnd;
    //extern uint16_t RamfuncsRunSize;
    //
    //extern uint16_t constLoadStart;
    //extern uint16_t constLoadEnd;
    //extern uint16_t constLoadSize;
    //extern uint16_t constRunStart;
    //extern uint16_t constRunEnd;
    //extern uint16_t constRunSize;
    
    //#define DEVICE_FLASH_WAITSTATES 2
    
    //*****************************************************************************
    //
    // Driver specific initialization code and macro.
    //
    //*****************************************************************************
    
    #define ETHERNET_NO_OF_RX_PACKETS   2U
    #define ETHERNET_MAX_PACKET_LENGTH 1538U
    
    #define NUM_PACKET_DESC_RX_APPLICATION PBUF_POOL_SIZE //8 - same as PBUF_POOL_SIZE
    
    
    Ethernet_Handle emac_handle;
    Ethernet_InitConfig *pInitCfg;
    uint32_t Ethernet_numRxCallbackCustom = 0;
    uint32_t releaseTxCount = 0;
    uint32_t genericISRCustomcount = 0;
    uint32_t genericISRCustomRBUcount = 0;
    uint32_t genericISRCustomROVcount = 0;
    uint32_t genericISRCustomRIcount = 0;
    
    Ethernet_Pkt_Desc  pktDescriptorRXCustom[NUM_PACKET_DESC_RX_APPLICATION];
    extern uint32_t Ethernet_numGetPacketBufferCallback;
    extern Ethernet_Device Ethernet_device_struct;
    uint8_t Ethernet_rxBuffer[ETHERNET_NO_OF_RX_PACKETS *
                              ETHERNET_MAX_PACKET_LENGTH];
    
    uint32_t sendPacketFailedCount = 0;
    
    uint8_t mac_custom[6] = {0xA8, 0x63, 0xF2, 0x00, 0x1D, 0x98};
    
    extern Ethernet_Pkt_Desc*
    lwIPEthernetIntHandler(Ethernet_Pkt_Desc *pPacket);
    
    
    
    
    // IPC
    #define IPC_CMD_GUI_COMMAND                 1001
    #define IPC_CMD_GUI_COMMAND_DATA_LENGTH     6
    
    #define IPC_CMD_PLOTS_COMMAND               1002
    #define IPC_CMD_PLOTS_COMMAND_DATA_LENGTH   14
    
    
    
    #define IPC_CMD_RESP            2001
    
    #pragma DATA_SECTION(commandToC28, "MSGRAM_CM_TO_CPU1")
    uint32_t commandToC28[50];
    
    
    
    //*****************************************************************************
    //
    // HTTP Webserver related callbacks and definitions.
    //
    //*****************************************************************************
    //
    // Currently, this implemented as a pointer to function which is called when
    // corresponding query is received by the HTTP webserver daemon. When more
    // features are needed to be added, it should be implemented as a separate
    // interface.
    //
    void httpLEDToggle(void);
    void(*ledtoggleFuncPtr)(void) = &httpLEDToggle;
    
    
    //*****************************************************************************
    //
    //  This function is a callback function called by the example to
    //  get a Packet Buffer. Has to return a ETHERNET_Pkt_Desc Structure.
    //  Rewrite this API for custom use case.
    //
    //*****************************************************************************
    Ethernet_Pkt_Desc* Ethernet_getPacketBufferCustom(void)
    {
        //
        // Get the next packet descriptor from the descriptor pool
        //
        uint32_t shortIndex = (Ethernet_numGetPacketBufferCallback + 3)
                    % NUM_PACKET_DESC_RX_APPLICATION;
    
        //
        // Increment the book-keeping pointer which acts as a head pointer
        // to the circular array of packet descriptor pool.
        //
        Ethernet_numGetPacketBufferCallback++;
    
        //
        // Update buffer length information to the newly procured packet
        // descriptor.
        //
        pktDescriptorRXCustom[shortIndex].bufferLength =
                                      ETHERNET_MAX_PACKET_LENGTH;
    
        //
        // Update the receive buffer address in the packer descriptor.
        //
        pktDescriptorRXCustom[shortIndex].dataBuffer =
                                          &Ethernet_device_struct.rxBuffer [ \
                   (ETHERNET_MAX_PACKET_LENGTH*Ethernet_device_struct.rxBuffIndex)];
    
        //
        // Update the receive buffer pool index.
        //
        Ethernet_device_struct.rxBuffIndex += 1U;
        Ethernet_device_struct.rxBuffIndex  = \
        (Ethernet_device_struct.rxBuffIndex%ETHERNET_NO_OF_RX_PACKETS);
    
        //
        // Receive buffer is usable from Address 0
        //
        pktDescriptorRXCustom[shortIndex].dataOffset = 0U;
    
        //
        // Return this new descriptor to the driver.
        //
        return (&(pktDescriptorRXCustom[shortIndex]));
    }
    
    //*****************************************************************************
    //
    //  This is a hook function and called by the driver when it receives a
    //  packet. Application is expected to replenish the buffer after consuming it.
    //  Has to return a ETHERNET_Pkt_Desc Structure.
    //  Rewrite this API for custom use case.
    //
    //*****************************************************************************
    Ethernet_Pkt_Desc* Ethernet_receivePacketCallbackCustom(
            Ethernet_Handle handleApplication,
            Ethernet_Pkt_Desc *pPacket)
    {
    
    	Ethernet_Pkt_Desc* temp_eth_pkt;
        //
        // Book-keeping to maintain number of callbacks received.
        //
    #ifdef ETHERNET_DEBUG
        Ethernet_numRxCallbackCustom++;
    #endif
    
    
    
          Ethernet_disableRxDMAReception(EMAC_BASE,0);
    
    
        //
        // This is a placeholder for Application specific handling
        // We are replenishing the buffer received with another buffer
        //
      //  return lwIPEthernetIntHandler(pPacket);
    
          temp_eth_pkt=lwIPEthernetIntHandler(pPacket);
    
    
          Ethernet_enableRxDMAReception(EMAC_BASE,0);
    
          return temp_eth_pkt;
    }
    
    void Ethernet_releaseTxPacketBufferCustom(
            Ethernet_Handle handleApplication,
            Ethernet_Pkt_Desc *pPacket)
    {
        //
        // Once the packet is sent, reuse the packet memory to avoid
        // memory leaks. Call this interrupt handler function which will take care
        // of freeing the memory used by the packet descriptor.
        //
        lwIPEthernetIntHandler(pPacket);
    
        //
        // Increment the book-keeping counter.
        //
    #ifdef ETHERNET_DEBUG
        releaseTxCount++;
    #endif
    }
    
    Ethernet_Pkt_Desc *Ethernet_performPopOnPacketQueueCustom(
                Ethernet_PKT_Queue_T *pktQueuePtr)
    {
        Ethernet_Pkt_Desc *pktDescHdrPtr;
    
        pktDescHdrPtr = pktQueuePtr->head;
    
        if(0U != pktDescHdrPtr)
        {
            pktQueuePtr->head = pktDescHdrPtr->nextPacketDesc;
            pktQueuePtr->count--;
        }
    
        return(pktDescHdrPtr);
    }
    void Ethernet_performPushOnPacketQueueCustom(
            Ethernet_PKT_Queue_T *pktQueuePtr,
            Ethernet_Pkt_Desc *pktDescHdrPtr)
    {
        pktDescHdrPtr->nextPacketDesc = 0U;
    
        if(0U == pktQueuePtr->head)
        {
            //
            // Queue is empty - Initialize it with this one packet
            //
            pktQueuePtr->head = pktDescHdrPtr;
            pktQueuePtr->tail = pktDescHdrPtr;
        }
        else
        {
            //
            // Queue is not empty - Push onto END
            //
            pktQueuePtr->tail->nextPacketDesc = pktDescHdrPtr;
            pktQueuePtr->tail        = pktDescHdrPtr;
        }
        pktQueuePtr->count++;
    }
    void Ethernet_setMACConfigurationCustom(uint32_t base, uint32_t flags)
    {
        HWREG(base + ETHERNET_O_MAC_CONFIGURATION) |= flags;
    }
    void Ethernet_clearMACConfigurationCustom(uint32_t base, uint32_t flags)
    {
        HWREG(base + ETHERNET_O_MAC_CONFIGURATION) &= ~flags;
    
    }
    
    interrupt void Ethernet_genericISRCustom(void)
    {
        genericISRCustomcount++;
        Ethernet_RxChDesc *rxChan;
        Ethernet_TxChDesc *txChan;
    //    Ethernet_HW_descriptor    *descPtr;
    //    Ethernet_HW_descriptor    *tailPtr;
        uint16_t i=0;
        Ethernet_clearMACConfigurationCustom(Ethernet_device_struct.baseAddresses.enet_base,ETHERNET_MAC_CONFIGURATION_RE);
        Ethernet_clearMACConfigurationCustom(Ethernet_device_struct.baseAddresses.enet_base,ETHERNET_MAC_CONFIGURATION_TE);
        for(i = 0U;i < Ethernet_device_struct.initConfig.numChannels;i++)
         {
             Ethernet_disableRxDMAReception(
                   Ethernet_device_struct.baseAddresses.enet_base,
                   i);
         }
        if(((ETHERNET_DMA_CH0_STATUS_AIS |
                             ETHERNET_DMA_CH0_STATUS_RBU) ==
                           (HWREG(Ethernet_device_struct.baseAddresses.enet_base +
                                  ETHERNET_O_DMA_CH0_STATUS) &
                                  (uint32_t)(ETHERNET_DMA_CH0_STATUS_AIS |
                                             ETHERNET_DMA_CH0_STATUS_RBU))) ||
              (ETHERNET_MTL_Q0_INTERRUPT_CONTROL_STATUS_RXOVFIS) ==
                                       (HWREG(Ethernet_device_struct.baseAddresses.enet_base +
                                              ETHERNET_O_MTL_Q0_INTERRUPT_CONTROL_STATUS) &
                                              (uint32_t)(ETHERNET_MTL_Q0_INTERRUPT_CONTROL_STATUS_RXOVFIS
                                                         )))
          {
              if((ETHERNET_DMA_CH0_STATUS_AIS |
                                 ETHERNET_DMA_CH0_STATUS_RBU) ==
                               (HWREG(Ethernet_device_struct.baseAddresses.enet_base +
                                      ETHERNET_O_DMA_CH0_STATUS) &
                                      (uint32_t)(ETHERNET_DMA_CH0_STATUS_AIS |
                                                 ETHERNET_DMA_CH0_STATUS_RBU)))
              {
              genericISRCustomRBUcount++;
              }
              if((ETHERNET_MTL_Q0_INTERRUPT_CONTROL_STATUS_RXOVFIS) ==
                      (HWREG(Ethernet_device_struct.baseAddresses.enet_base +
                             ETHERNET_O_MTL_Q0_INTERRUPT_CONTROL_STATUS) &
                             (uint32_t)(ETHERNET_MTL_Q0_INTERRUPT_CONTROL_STATUS_RXOVFIS
                                        )))
              {
                  genericISRCustomROVcount++;
                  Ethernet_enableMTLInterrupt(Ethernet_device_struct.baseAddresses.enet_base,0,
                                              ETHERNET_MTL_Q0_INTERRUPT_CONTROL_STATUS_RXOVFIS);
              }
    
            /*
                 * Clear the AIS and RBU status bit. These MUST be
                 * cleared together!
                 */
                Ethernet_clearDMAChannelInterrupt(
                        Ethernet_device_struct.baseAddresses.enet_base,
                        ETHERNET_DMA_CHANNEL_NUM_0,
                        ETHERNET_DMA_CH0_STATUS_AIS |
                        ETHERNET_DMA_CH0_STATUS_RBU);
    
                /*
               *Recover from Receive Buffer Unavailable (and hung DMA)
             *
             * All descriptor buffers are owned by the application, and
             * in result the DMA cannot transfer incoming frames to the
             * buffers (RBU condition). DMA has also entered suspend
             * mode at this point, too.
             *
             * Drain the RX queues
             */
    
                /* Upon RBU error, discard all previously received packets */
                if(Ethernet_device_struct.initConfig.pfcbDeletePackets != NULL)
                    (*Ethernet_device_struct.initConfig.pfcbDeletePackets)();
    
                rxChan =
                   &Ethernet_device_struct.dmaObj.rxDma[ETHERNET_DMA_CHANNEL_NUM_0];
                txChan=
                   &Ethernet_device_struct.dmaObj.txDma[ETHERNET_DMA_CHANNEL_NUM_0];
    
        /*
         * Need to disable multiple interrupts, so protect the code to do so within
         * a global disable block (to prevent getting interrupted in between)
         */
    
                if(NULL!= Ethernet_device_struct.ptrPlatformInterruptDisable)
                {
                    (*Ethernet_device_struct.ptrPlatformInterruptDisable)(
                        Ethernet_device_struct.interruptNum[
                            ETHERNET_RX_INTR_CH0 + rxChan->chInfo->chNum]);
    
                    (*Ethernet_device_struct.ptrPlatformInterruptDisable)(
                        Ethernet_device_struct.interruptNum[
                            ETHERNET_GENERIC_INTERRUPT]);
                }
                /* verify we have full capacity in the descriptor queue */
                if(rxChan->descQueue.count < rxChan->descMax) {
                  /* The queue is not at full capacity due to OOM errors.
                  Try to fill it again */
                    Ethernet_addPacketsIntoRxQueue(rxChan);
                }
                Ethernet_initRxChannel(
                        &Ethernet_device_struct.initConfig.chInfo[ETHERNET_CH_DIR_RX][0]);
    
                Ethernet_writeRxDescTailPointer(
                    Ethernet_device_struct.baseAddresses.enet_base,
                    0,
                    (&Ethernet_device_struct.rxDesc[
                     ((uint32_t)ETHERNET_DESCRIPTORS_NUM_RX_PER_CHANNEL) *
                      (0 + (uint32_t)1U)]));
    
                if(NULL!= Ethernet_device_struct.ptrPlatformInterruptEnable)
                {
                    (*Ethernet_device_struct.ptrPlatformInterruptEnable)(
                        Ethernet_device_struct.interruptNum[
                            ETHERNET_RX_INTR_CH0 + rxChan->chInfo->chNum]);
                    (*Ethernet_device_struct.ptrPlatformInterruptEnable)(
                        Ethernet_device_struct.interruptNum[
                            ETHERNET_GENERIC_INTERRUPT]);
                }
    
    
        }
        if(0U != (HWREG(Ethernet_device_struct.baseAddresses.enet_base +
                                     ETHERNET_O_DMA_CH0_STATUS) &
                               (uint32_t) ETHERNET_DMA_CH0_STATUS_RI))
        {
            genericISRCustomRIcount++;
            Ethernet_clearDMAChannelInterrupt(
                            Ethernet_device_struct.baseAddresses.enet_base,
                            ETHERNET_DMA_CHANNEL_NUM_0,
                            ETHERNET_DMA_CH0_STATUS_NIS | ETHERNET_DMA_CH0_STATUS_RI);
        }
    
        for(i = 0U;i < Ethernet_device_struct.initConfig.numChannels;i++)
         {
             Ethernet_enableRxDMAReception(
                   Ethernet_device_struct.baseAddresses.enet_base,
                   i);
         }
        Ethernet_setMACConfigurationCustom(Ethernet_device_struct.baseAddresses.enet_base,ETHERNET_MAC_CONFIGURATION_RE);
        Ethernet_setMACConfigurationCustom(Ethernet_device_struct.baseAddresses.enet_base,ETHERNET_MAC_CONFIGURATION_TE);
    }
    
    void
    Ethernet_init(const unsigned char *mac)
    {
        Ethernet_InitInterfaceConfig initInterfaceConfig;
        uint32_t macLower;
        uint32_t macHigher;
        uint8_t *temp;
    
        initInterfaceConfig.ssbase = EMAC_SS_BASE;
        initInterfaceConfig.enet_base = EMAC_BASE;
        initInterfaceConfig.phyMode = ETHERNET_SS_PHY_INTF_SEL_MII;
    
        //
        // Assign SoC specific functions for Enabling,Disabling interrupts
        // and for enabling the Peripheral at system level
        //
        initInterfaceConfig.ptrPlatformInterruptDisable =
                                                        &Platform_disableInterrupt;
        initInterfaceConfig.ptrPlatformInterruptEnable =
                                                         &Platform_enableInterrupt;
        initInterfaceConfig.ptrPlatformPeripheralEnable =
                                                        &Platform_enablePeripheral;
        initInterfaceConfig.ptrPlatformPeripheralReset =
                                                         &Platform_resetPeripheral;
    
        //
        // Assign the peripheral number at the SoC
        //
        initInterfaceConfig.peripheralNum = SYSCTL_PERIPH_CLK_ENET;
    
        //
        // Assign the default SoC specific interrupt numbers of Ethernet interrupts
        //
        initInterfaceConfig.interruptNum[0] = INT_EMAC;
        initInterfaceConfig.interruptNum[1] = INT_EMAC_TX0;
        initInterfaceConfig.interruptNum[2] = INT_EMAC_TX1;
        initInterfaceConfig.interruptNum[3] = INT_EMAC_RX0;
        initInterfaceConfig.interruptNum[4] = INT_EMAC_RX1;
    
        pInitCfg = Ethernet_initInterface(initInterfaceConfig);
    
        Ethernet_getInitConfig(pInitCfg);
        pInitCfg->dmaMode.InterruptMode = ETHERNET_DMA_MODE_INTM_MODE2;
    
        //
        // Assign the callbacks for Getting packet buffer when needed
        // Releasing the TxPacketBuffer on Transmit interrupt callbacks
        // Receive packet callback on Receive packet completion interrupt
        //
        pInitCfg->pfcbRxPacket = &Ethernet_receivePacketCallbackCustom;
        pInitCfg->pfcbGetPacket = &Ethernet_getPacketBuffer;    //custom
        pInitCfg->pfcbFreePacket = &Ethernet_releaseTxPacketBufferCustom;
    
        //
        //Assign the Buffer to be used by the Low level driver for receiving
        //Packets. This should be accessible by the Ethernet DMA
        //
        pInitCfg->rxBuffer = Ethernet_rxBuffer;
    
        //
        // The Application handle is not used by this application
        // Hence using a dummy value of 1
        //
        Ethernet_getHandle((Ethernet_Handle)1, pInitCfg , &emac_handle);
    
        //
        // Disable transmit buffer unavailable and normal interrupt which
        // are enabled by default in Ethernet_getHandle.
        //
        Ethernet_disableDmaInterrupt(Ethernet_device_struct.baseAddresses.enet_base,
                                     0, (ETHERNET_DMA_CH0_INTERRUPT_ENABLE_TBUE |
                                         ETHERNET_DMA_CH0_INTERRUPT_ENABLE_NIE));
    
        //
        // Enable the MTL interrupt to service the receive FIFO overflow
        // condition in the Ethernet module.
        //
        Ethernet_enableMTLInterrupt(Ethernet_device_struct.baseAddresses.enet_base,0,
                                    ETHERNET_MTL_Q0_INTERRUPT_CONTROL_STATUS_RXOIE);
    
        //
        // Disable the MAC Management counter interrupts as they are not used
        // in this application.
        //
        HWREG(Ethernet_device_struct.baseAddresses.enet_base + ETHERNET_O_MMC_RX_INTERRUPT_MASK) = 0xFFFFFFFF;
        HWREG(Ethernet_device_struct.baseAddresses.enet_base + ETHERNET_O_MMC_IPC_RX_INTERRUPT_MASK) = 0xFFFFFFFF;
        //
        //Do global Interrupt Enable
        //
        (void)Interrupt_enableInProcessor();
    
        //
        //Assign default ISRs
        //
        Interrupt_registerHandler(INT_EMAC_TX0, Ethernet_transmitISR);
        Interrupt_registerHandler(INT_EMAC_RX0, Ethernet_receiveISR);
        Interrupt_registerHandler(INT_EMAC, Ethernet_genericISRCustom);
    
        //
        // Convert the mac address string into the 32/16 split variables format
        // that is required by the driver to program into hardware registers.
        // Note: This step is done after the Ethernet_getHandle function because
        //       a dummy MAC address is programmed in that function.
        //
        temp = (uint8_t *)&macLower;
        temp[0] = mac[0];
        temp[1] = mac[1];
        temp[2] = mac[2];
        temp[3] = mac[3];
    
        temp = (uint8_t *)&macHigher;
        temp[0] = mac[4];
        temp[1] = mac[5];
    
        //
        // Program the unicast mac address.
        //
        Ethernet_setMACAddr(EMAC_BASE,
                            0,
                            macHigher,
                            macLower,
                            ETHERNET_CHANNEL_0);
    
        Ethernet_clearMACConfigurationCustom(Ethernet_device_struct.baseAddresses.enet_base,ETHERNET_MAC_CONFIGURATION_RE);
        Ethernet_setMACConfigurationCustom(Ethernet_device_struct.baseAddresses.enet_base,ETHERNET_MAC_CONFIGURATION_RE);
    }
    
    
    
    void udp_rx_callback(void *arg, struct udp_pcb *upcb, struct pbuf *p,
                   struct ip_addr *addr, u16_t port)
    
    {
        char *cad_rx;
        uint16_t long_actual = 0;
        uint16_t long_UDP_complete = 0;
        uint16_t long_total = 0;
        uint8_t cnt_lee = 0;
    
        httpLEDToggle();
    
        memset(buf_rx, 0x00, 50);
    
        long_total = p->tot_len;
    
        cont_rx_udp++;
    
        while ((long_UDP_complete < long_total)
                && (long_UDP_complete < 1800) || (cnt_lee == 0))
        {
            cnt_lee++;
            long_actual = p->len;
    
            cad_rx = p->payload;
    
            int i = 0;
            for (i = 0; i < long_actual; i++)
            {
    
                buf_rx[0 + i + long_UDP_complete] = *cad_rx++;
            }
            long_UDP_complete = long_actual + long_UDP_complete;
            buf_rx[long_UDP_complete + 1] = '\n';
    
            if (long_UDP_complete == long_total)
            {
                pbuf_free(p); /* don't leak the pbuf!*/
            }
            else
            {
                if ( p->next != NULL)
                p = p->next;
                //  pbuf_free(a);                                   /* don't leak the pbuf!*/
            }
    
    //        if ((buf_rx[0] == 'S') && (buf_rx[1] == 'T') && (buf_rx[2] == 'O') && (buf_rx[3] == 'P'))
    //        {                    //Disconnect
    //                             //udp_disconnect(upcb);
    //
    //            Connected_udp_28000 = false;
    //        }
    //        else if ((buf_rx[0] == 'S') && (buf_rx[1] == 'T') && (buf_rx[2] == 'A') && (buf_rx[3] == 'R') && (buf_rx[4] == 'T'))
    //        {                //Connect
    //
    //                    Connected_udp_28000 = true;
    //
    //                   /* process the payload in p->payload */
    //                   udp_connect(upcb, addr, port); /* connect to the remote host */
    //
    //        }
        }
    
        pbuf_free(p);
    
        int x;
        bool send_to_c28 = false;
        uint32_t ipc_len = 0;
        uint32_t ipc_command = 0;
    
        if (arg == 1001) {
    
            send_to_c28 = true;
            ipc_command = IPC_CMD_GUI_COMMAND;
            ipc_len = IPC_CMD_GUI_COMMAND_DATA_LENGTH;
    
            switch(buf_rx[2])
            {
            // Pan.
            case 0x01:
                cnt_Command_Pan++;
                break;
                // Tilt.
            case 0x02:
                cnt_Command_Tilt++;
                break;
                // Zoom.
            case 0x04:
                cnt_Command_Zoom++;
                break;
                // Commands.
            case 0x05:
    
    
                if (arg == 1001) {
                    switch(buf_rx[3])
                    {
                    case 3:
                        sendTo1 = 3;
                        break;
                    case 4:
                        sendTo1 = 4;
                        break;
    
                    }
    
                    if (sendTo1 != 0) {
                        //                udp_connect(g_upcb_GUI, addr, port); /* connect to the remote host */
                        udp_connect(g_upcb_Decoder, addr, 14001); /* connect to the remote host */
                    }
                }
    
    
                cnt_Command_Commands++;
                break;
            } // Switch
    
    
        } // if (arg == 1001)
        else if (arg == 1002) {
            send_to_c28 = true;
            ipc_command = IPC_CMD_PLOTS_COMMAND;
            ipc_len = IPC_CMD_PLOTS_COMMAND_DATA_LENGTH;
        }
    
        // Check if we need to send the data to the C28 Core.
        if (send_to_c28 == true) {
            send_to_c28 = false;
    
            // Copy the data to a buffer at the MSGRAM_CM_TO_CPU1 memory section.
            // TODO: test size of buffer.
            for (x=0; x<ipc_len; x++)
            {
                commandToC28[x] = buf_rx[x];
            }
    
            // Send the command to C28 core.
            IPC_sendCommand(IPC_CM_L_CPU1_R, IPC_FLAG0, IPC_ADDR_CORRECTION_ENABLE,
                            ipc_command, (uint32_t)commandToC28, ipc_len);
        }
    
    
    
    //    IPC_waitForAck(IPC_CM_L_CPU1_R, IPC_FLAG0);
    
        // Read response
    //    if(IPC_getResponse(IPC_CM_L_CPU1_R) == TEST_PASS);
    
    
    //    if (!Connected_udp_28000)
    //    {
    //        udp_disconnect(upcb);
    //    }
    
    }
    
    /* UDP initialization ......................................................*/
    void my_udp_init(void)
    {
        g_upcb_GUI = udp_new();
        udp_bind(g_upcb_GUI, IP_ADDR_ANY, 1001);
        udp_recv(g_upcb_GUI, &udp_rx_callback, (void*) 1001);
    
        g_upcb_Plots = udp_new();
        udp_bind(g_upcb_Plots, IP_ADDR_ANY, 1002);
        udp_recv(g_upcb_Plots, &udp_rx_callback, (void*) 1002);
    
        g_upcb_Decoder = udp_new();
        udp_bind(g_upcb_Decoder, IP_ADDR_ANY, 14001);
        udp_recv(g_upcb_Decoder, &udp_rx_callback, (void*) 14001);
    
    
    //    unsigned long IPAddr =  0x0A0101C0UL;
    //    const ip_addr_t *ipaddr = &IPAddr;
    //    udp_connect(g_upcb_GUI, ipaddr, 1001); /* connect to the remote host */
    //    udp_connect(g_upcb_Decoder, ipaddr, 14001); /* connect to the remote host */
    }
    
    
    //*****************************************************************************
    //
    // This example demonstrates the use of the Ethernet Controller.
    //
    //*****************************************************************************
    
    unsigned long IPAddr =  0xC0010105UL; // 0xC0A80004; //192.168.0.4
    unsigned long NetMask = 0xFFFFFF00;
    unsigned long GWAddr = 0x00000000;
    
    
    void main_Ethernet_Init(void)
    {
        unsigned long ulUser0, ulUser1;
        unsigned char pucMACArray[8];
    
        int i=0;
    
        // Set user/company specific MAC octets
        // (for this code we are using A8-63-F2-00-00-80)
        // 0x00 MACOCT3 MACOCT2 MACOCT1
        ulUser0 = 0x00F263A8;
    
        // 0x00 MACOCT6 MACOCT5 MACOCT4
        ulUser1 = 0x00800000;
    
        //
        // Convert the 24/24 split MAC address from NV ram into a 32/16 split MAC
        // address needed to program the hardware registers, then program the MAC
        // address into the Ethernet Controller registers.
        //
        pucMACArray[0] = ((ulUser0 >>  0) & 0xff);
        pucMACArray[1] = ((ulUser0 >>  8) & 0xff);
        pucMACArray[2] = ((ulUser0 >> 16) & 0xff);
        pucMACArray[3] = ((ulUser1 >>  0) & 0xff);
        pucMACArray[4] = ((ulUser1 >>  8) & 0xff);
        pucMACArray[5] = ((ulUser1 >> 16) & 0xff);
    
        //
        // Initialize ethernet module.
        //
        Ethernet_init(pucMACArray);
    
        //
        // Initialze the lwIP library, using DHCP.
        //
        lwIPInit(0, pucMACArray, IPAddr, NetMask, GWAddr, IPADDR_USE_STATIC);
    
        // Initialize the UDP server
        //
        my_udp_init();
    
        //
        // Loop forever. All the work is done in interrupt handlers.
        //
         uint32_t cnt_FFT = 0;
    
        Interrupt_setPriority(INT_EMAC_TX0, 2);
        Interrupt_setPriority(INT_EMAC_RX0, 1);
        Interrupt_enable(INT_EMAC_TX0);
        Interrupt_enable(INT_EMAC_RX0);
        Interrupt_enable(INT_EMAC);
    
        volatile int cnt_total_loop=0;
        volatile int cnt_total_mqtt_pub=0;
    
    
    
        IPC_clearFlagLtoR(IPC_CM_L_CPU1_R, IPC_FLAG_ALL);
    
        IPC_sync(IPC_CM_L_CPU1_R, IPC_FLAG31);
    
        while (1)
        {
            cnt_total_loop++;
    
    //        if (Connected_udp_28000)
            if (sendTo1 || sendTo2)
            {
            	//UDP TX block
    
                if (flag_TX_frame_UDP)
                {
                	cnt_FFT++;
    
                	//flag_TX_frame_UDP = false;
    
                	/////////////////////////////////////////////
                	for (i = 0; i < PAYLOAD; i++)
                    {
                	    if(i < buf_tx_start_msg_count) {
                	        buf_tx[i] = (uint8_t)buf_tx_start_msg[i];
                	    } else {
                            buf_tx[i] = (uint8_t) (cnt_FFT);
                	    }
    
                    }
                	buf_tx[0] = 0x51;
                	buf_tx[1] = 0xAC;
                	buf_tx[2] = 0x08;
                	buf_tx[3] = 0xA4;
                	buf_tx[4] = 0x00;
                	buf_tx[5] = (sendTo1==3)?2:0;
                	buf_tx[6] = 0x02;
                	buf_tx[7] = 0x00;
                	buf_tx[8] = 0x04;
                	buf_tx[9] = 0x00;
                	buf_tx[10] = (sendTo1==3)?0x0E:0x8D;
    
                	////////////////////////////////////////////
    
    //                pbuf1_tx = pbuf_alloc(PBUF_TRANSPORT, 11, PBUF_RAM);
                    pbuf1_tx = pbuf_alloc(PBUF_TRANSPORT, PAYLOAD, PBUF_RAM);
                    if (pbuf1_tx!= NULL) {
    
                    pbuf1_tx->payload = (void*) buf_tx;
    //                pbuf1_tx->tot_len = PAYLOAD;  //17        // long_UDP_complete+4;
    //                pbuf1_tx->len = PAYLOAD;   //17       // long_UDP_complete+4;
    
                    pbuf1_tx->tot_len = 11;  //17        // long_UDP_complete+4;
                    pbuf1_tx->len = 11;   //17       // long_UDP_complete+4;
    
                    if (sendTo1) {
                        udp_send(g_upcb_Decoder, pbuf1_tx);
                        udp_disconnect(g_upcb_Decoder);
    
                        sendTo1 = 0;
                    }
                    else {
    //                    if (sendTo2) {
    //                        udp_send(g_upcb_Plots, pbuf1_tx);
    //                        sendTo2 = false;
    //                        udp_disconnect(g_upcb_Plots);
    //                    }
                    }
                    }
    
    
                    if (pbuf1_tx!= NULL)
                    pbuf_free(pbuf1_tx);
    
                }
    
            }
    
    
            SysCtl_delay(6000000);//aprox 1 sec
    
            sys_check_timeouts();
    
        }
    }
    
    //*****************************************************************************
    //
    // Called by lwIP Library. Toggles the led when a command is received by the
    // HTTP webserver.
    //
    //*****************************************************************************
    void httpLEDToggle(void)
    {
        //
        // Toggle the LED D1 on the control card.
        //
    //    GPIO_togglePin(DEVICE_GPIO_PIN_LED1);
    }
    
    
    //*****************************************************************************
    //
    // Called by lwIP Library. Could be used for periodic custom tasks.
    //
    //*****************************************************************************
    
    uint32_t cnt_ms_lwip_Htimer=0;
    uint32_t cnt_ms_TX_Htimer=0;
    void lwIPHostTimerHandler(void)
    {
    //	msTime++;
    
    	cnt_ms_lwip_Htimer++;
    }
    
    

  • Givon,

    Will take a look at the code that you shared and get back to you.

    Best Regards

    Siddharth

  • Givon, 

    Were you able to resolve this ?  

    Best Regards

    Siddharth