This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280039C: When set 65535 to TZCLR register, the TZCLR.CBCPULSE would set as 0x03, why not 0x0?

Part Number: TMS320F280039C

Hi Champs,

I am asking for my customer here! Thanks~

Here are the below code.

EPWM_setTripZoneAction(EPWM1_BASE, EPWM_TZ_ACTION_EVENT_TZA, EPWM_TZ_ACTION_LOW); //
EPWM_setTripZoneAction(EPWM1_BASE, EPWM_TZ_ACTION_EVENT_TZB, EPWM_TZ_ACTION_LOW); //

//Trip4 will be active if CMPSSL & CMPSSH is active
EPWM_selectDigitalCompareTripInput(EPWM1_BASE, EPWM_DC_TRIP_TRIPIN4, EPWM_DC_TYPE_DCBH); //DCBEVT2
EPWM_setTripZoneDigitalCompareEventCondition(EPWM1_BASE, EPWM_TZ_DC_OUTPUT_B2, EPWM_TZ_EVENT_DCXH_HIGH); //
EPWM_setDigitalCompareEventSource(EPWM1_BASE, EPWM_DC_MODULE_B, EPWM_DC_EVENT_2, EPWM_DC_EVENT_SOURCE_ORIG_SIGNAL);//
EPWM_selectCycleByCycleTripZoneClearEvent(EPWM1_BASE, EPWM_TZ_CBC_PULSE_CLR_CNTR_ZERO); //

//Enable the following trips. Add Emu stop.
EPWM_enableTripZoneSignals(EPWM1_BASE, EPWM_TZ_SIGNAL_DCBEVT2);

// Clear any spurious trip
EPWM_clearTripZoneFlag(EPWM1_BASE, (EPWM_TZ_FLAG_OST |EPWM_TZ_FLAG_CBC | EPWM_TZ_FLAG_DCBEVT2 | EPWM_TZ_OST_FLAG_DCBEVT1)); //EPWM_TZ_FLAG_DCAEVT2 |

#1. Trip occurs, Debug with the normal conditions, not write the 65535 to TZCLR. it works normally

#2. Trip occurs, Debug with the conditions, write the 65535 to TZCLR. And then TZCLR.CBCPULSE would set as 0x03, so it would not clear automatically.

So it would not CBC protection as show below 

The customer is confused. Using 65535 to clear the TZCLR register will affect the value of the high bit/TZCLR.CBCPULSE? Thanks a lot!

  • Hello Shaoxing,

    TZCLR[13:7] bits are reserved as per the TRM, and writing values to them can result in undefined behavior. Does this still occur if writing 0xC07F?

    Regards,

    Jason Osborn

  • Hi Jason,

    When TZCLR set as 0xC07F, and TZCLR.CBCPULSE would still set as 0x03. Thanks~

     

  • Hello Shaoxing,

    Re-reading this, you are intending to set TZCLR[CBCPULSE] to [00], [01], or [10], and it is being set to [11], correct? Either the original write (0xFFFF) or the version that avoids reserved registers (0xC07F) will write [11] to that register. Apologies for not realizing the thread intent earlier.

    Essentially, TZCLR[CBCPULSE] has different behavior to the other TZCLR bits. In order to set that bit properly, instead adjust the hex value being written to substitute the correct bit pattern, for example, 0xC07F -> 0x407F for [01] bit pattern on TZCLR[CBCPULSE], which clears the CBC trip latch on CTR = PRD.

    Hope that helps,

    Jason Osborn