Part Number: TMS320F280039C
I am using the MCAN module for transmitting and receiving CAN 2.0 A frames. Because of the noise bus, Node is facing stuffing and form errors. I need to implement auto bus recovery, but there is no precise implementation with the driver library. For DCAN ABO bit in CTL reg can enable autobus recovery, How can we do the same for MCAN??