We have an application, which is the main application with DSP BIOS, running in the internal flash. We have an other application in external flash, which worked as boot loader and no DSP BIOS. These two applications are total independed.
Both of the two applications can receive commands from RS232/USB. When the main application is running in the internal flash, we send the command to let it jump to the external flash to run the boot loader code. We use this
asm
The problem is after the main application received the command, execute the asm(" LB #0x00298064"), the F28235 didn't run the boot loader code, it reset itself and run the main application again.
Who knows why? and how to get it work.
We know the boot loader code in the external flash works and 0x00298064 is the valid entry point address.
Becasue that if we run a small application, which no DSP BIOS, in the internal falsh instead of the main application, when it receive the command and excute the jump asm(" LB #0x00298064"), the boot loader in the external flash can start to run without problem.
Thanks,
Anna