Dear All,
I am using the GPIO8_x2 as an LED . According to data sheet ,it uses INTOSC2 for configuration but even by proceeding that way still its not working in continuous run , but if I use breakpoints on the LED then it glows.
Regards
Shivani
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear All,
I am using the GPIO8_x2 as an LED . According to data sheet ,it uses INTOSC2 for configuration but even by proceeding that way still its not working in continuous run , but if I use breakpoints on the LED then it glows.
Regards
Shivani
Hi Shivani,
Thanks for your question. If this is working with breakpoints, it actually sounds like the LED is toggling too fast to see (with majority of time in low level). Please use a scope or logic analyzer and provide a capture of the GPIO8 pin for us to debug further.
Regards,
Vince