Part Number: TMS320F280025
Other Parts Discussed in Thread: UCC28180, UCC24624, UCC27714, TIDM-02013
Hii,
I am working on a 750 W battery charger project.
PFC topology
- Boost topology with UCC28180 control IC from Texas instruments.
- Switching frequency is 105khz
DC-DC topology
- LLC half bridge converter(Split cap configuration) with secondary synchronous Mosfet.
- Digital control technology is implemented using C2000 series MCU
- Secondary side synchronous Mosfet drive is implemented through UCC24624.
- Gate driver is UCC27714
- Operating frequency range is from 93khz to 200khz
- Resonant frequency is 153khz
- Lm= 110uH,Lr = 27uH ,Cr= 40nF
- Dead time is around 220nSec
Problem statement
- During the standalone load test of individual converter, both converters are working perfectly fine with desired performance.
- For standalone LLC testing , i am applying the pulses (250khz) to both high & low side mosfets first & then apply 390 V DC at the input.
- When I am integrating both PFC & LLC , & apply 230Vac at the input there is a gate driver & mosfet failure of LLC converter at the starting itself with out any load.
- LLC mosfet pulses are applied with a particular frequency(250khz) before 230V is applied in integration testing. As the power supply is independent of the input 230V supply.
Is it happening due to absence in softstart mechanism for LLC ?? If it is the reason, then why it is not failing in standalone testing