Other Parts Discussed in Thread: BOOST-DAC8568, MSP430F5529, DAC128S085EVM, DAC8568
Hi,
Good Day.
We have a Delfino F28379D Launchpad board and are wondering about compatibility with the BOOST-DAC8568 Booster Pack.
The Delfino board already has 3DACs on board but we would like at least 8 more in adding the booster pack can we also have access to the 20 ADC channels?
So we are wanting to use the Delfino launch pad board for a multi-channel Active noise control system, so in real-time receiving data through multiple ADCs and sending data to multiple DACs. The point of this inquiry is we need more DACs than are currently available, would this booster pack be compatible (BOOST-DAC8568) and give us additional outputs to the current 3 on the board? How many ADC channels can we have with the current Delfino F28379D Launchpad board? And do you offer any other products which would achieve this?
I have looked but the boost pack documentation only has the MSP430F5529 microcontroller LaunchPad as the example, and it doesn't come under the F28379D documentation.
Although it's the same pin layout so should it just work fine.
Please advise. Thank you very much.
Best Regards,
Ray Vincent