Other Parts Discussed in Thread: SYSCONFIG
Hi Champ,
I am asking for my customer.
Recently, my customer is facing an issue on there is no EPWM output (EPWM5) from the pins (directly measuring both A/B channels, disconnect the part with EPWM). They have seen the failure on few pcs.
It has been verified the EPWM configuration is ok since copy the same configuration to other sets of EPWM, there are PWM outputs from both channels.
Besides, it is quite weird that both channels on EPWM5 can't output PWM signal, but both pins (A/B channels) are normal if they are configured to GPIO, able to set high / low.
Customer can't do the A-B-A swap because it might damage the device when desoldering the device from PCB.
So far, the only thing that I could think about is there might be a voltage larger than 0.3V + VDDIO on those pins or reverse current sinking from output to the pins that could damage the EPWM peripheral.
Has any expert ever seen this kind of scenario ? What might be other root cause, welcome for any suggestion ?
Thanks and regards,
Johnny