This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I used this code: C:\ti\c2000\C2000Ware_5_00_00_00\driverlib\f2838x\examples\c28x\epwm\CCS
I am working with the docking station and TMS320F28388D.
I work for example with epwm3 and didnt see any dead time.
Why?
Hi Ben,
I assume you are specifically looking for deadband support. Each example support in C2000ware is to help with intital evaluation as a starting point.
\
You can refer to the ex:8 in EPWM, below is how the example is configured
This help for DB configuration. If something else, please share the snip shots of the waveform here for further support.
Thanks & Regards,
Uttam
The deadband example explains between multiple EPWM. Inorder to enable DB between EPWM_1A and EPWM_1B this will be done by setting rising edge and falling edge delay enabling