Other Parts Discussed in Thread: PMP23126, TIDM-02013, SFRA
Good Evening,
We are in need of DCDC- Bidirectional which will be used in 400V/800V EV system, Kindly share any reference design which we can have a headstart on this requriements.
1. V Max = 420V-800V -Vin to 12V Vout (Vice versa)
2. I Max = 300Amps
3. P Max = 3.6 KW
We need AC-DC connverter as well
1. VAC in = 85 to 260V
2. I-In @100V = 16 Amps
3. Freq = 47 -63 Hz
4. DC Out = 200V to 450V DC
5. DC out Max current = 30 Amps
We are planning to incorporate both in single enclosure but different PCBAs and seperate external interfaces.
Regards,
Muthuraj M