Hello TI Team.
I have a question about DC flyback PWM configuration. Why are they configured in slave mode instead of master mode?
PWM_1ch_UpDwnCnt_CNF(3, (CPU_FREQ / (FLYBACK_FREQ)), 0, (CPU_FREQ / (FLYBACK_FREQ * 2)) - 2);
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello TI Team.
I have a question about DC flyback PWM configuration. Why are they configured in slave mode instead of master mode?
PWM_1ch_UpDwnCnt_CNF(3, (CPU_FREQ / (FLYBACK_FREQ)), 0, (CPU_FREQ / (FLYBACK_FREQ * 2)) - 2);
We are using PWM1 for the inverter stage. So that is the master. The flyback uses PWM3 and so it is the slave.
Hi Shamim Choudhury ok, I understand and thank you for information. In this case, I have another question about PWM3 configuration. Right now the channel B of PWM3 have a dead-band configuration.
I want to connect my second DC-flayback to this channel to have two DC flybacks per one PV panel but channel B should be 180 degree phase shifted than channel A.
Could you help me with this configuration to have PWM3B phase shifted 180 degree than PMW3A?
Use the complimentary config for PWM3. Then A and B channels will be 180 deg out of phase
Use AQ module to set PWM3A high and PWM3B low. See the Tech Ref Manual (one of pages shown below)