Hi All,
I am working on TMS320F28375S using driverlib api's of C2000 ware SDK in Code Composer Studio.
SPI communication to slave device was successful at 40 MHz clock in RAM environment using Generic RAM linker file.
When environment is changed to FLASH using Generic Flash linker file, SPI clock frequency was observed to be maximum of 11.5 MHz only, but i need SPI clock frequency to be 40 MHz in FLASH environment to communicate with slave device.
Please suggest some solution to resolve the issue.
Thanks in Advance,
Arun Badiger