Part Number: TIDM-BIDIR-400-12
Hello, Teams,
Thank you for continuing to give me advice for prototyping TIDM-BIDIR-400-12.
I’d like to ask the below questions about PR798 produced by TI.
- According to the schematics of TIDM-BIDIR-400-12 drawn in 12/16/2010 and the schematics of PR798 drawn in 7/26/2011, I assume that some connections or pinouts are inconsistent. Would you mind showing me the latest and correct connections or pinouts, and sharing me the latest, detailed schematics of TIDM-BIDIR-400-12 and PR798?
- Is PR798 sold? Or I’d like to know the information of the substitute one.
- If both PR798 and the substitute one are not sold, I anticipate that I have to redesign the circuit and the PCB of PR798. Is it correct? Is it able for me to get the CAD files and the BOM?
I appreciate your every support.
Best Regards,
Takumi