This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Background: I was trying to load the complied program 2XPM_Sensorless(flash option) from controlsuite into F28035 controlcard. I have observed follwing problems:
1. Error: failed to load program '2XPM_Sensorless.out' on traget 'Spectrum Digital XDS 510USB Emulator_0/C28xx' - during load program
2. This project contains unresolved buildable linked resources. It might not build as expected. - during project build
I checked the following
1. I created a target configuration with XDS510USB emulator and selected piccolo control card for F28035
2. In bedug window, tool option, I saw thw gel file is f28035.gel is success
3. However I do not see anything in tool, onchip flash window.
Can somebody help me what else I need to do so that I can compile the program for flash and load it properly ?
Chakrabarti,
Please clarify the following:
Regards,
Manoj
yes
CCSV4.0
LVMultiAxis+PfcKit_v1.4 directory in controlsuite, its 2XPM_Sensorless
Are you talking about : F28035_FLASH_2xPM_Sensorless.CMD file that is there in the window ?
linker error: failed to load program '2XPM_Sensorless.out' on traget 'Spectrum Digital XDS 510USB Emulator_0/C28xx'
Build problem: This project contains unresolved buildable linked resources. It might not build as expected
Not sure why you see the problem. I just downloaded the project you mentioned from the control suite and was able to successfully build the project without making any modification.
Regards,
Manoj