The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28335: usage of ADC driver amplifier OPA325 vs TLV6001

Part Number: TMS320F28335
Other Parts Discussed in Thread: OPA325, TLV6001

Dear Experts,

I am working on a customized TMS320F28335 board. There are some final things that I want to get clarified. There is a section of circuit that conditions +/-4V signal to 0-3V  that is connected to the analog pins of micrcontroller. I have a doubt in this regard. There are two TI links that you can find on this page. The first one uses TLV600X that converts differnetial to single ended and the same output can be connected directly to the ADC pin. On the other hand, OPA325 is a recommended IC to use as a ADC driver.

Would you recommend to use a single TLV600X that functions as a conditioner as well as a ADC driver, or use another OPA325 or TLV600X to use a buffer?

Or else can I use the single TLV600 circuit(scaling and shifting) and an RC circuit at the output.

TI's differential to single ended recommendation link  OPA325 link

Regards,

Rajesh BN.