Part Number: TMS320F280025C
Other Parts Discussed in Thread: UNIFLASH
Hi,
I am getting error while unlocking the memory with CSM password via uniflash.
I followed below steps;
1. Configured CSM password for zone 1 and flashed the code via ccs.
2. After power cycle , I tried connecting it via uniflash, I entered correct password and clicked on unlock.
3. But I am getting error while connecting.
So, do we need to modify the target configuration file or gel file in order to be able to connect the controller via JTAG?
If yes, then what are those configurations?
We tried this on our PCB, hence it is difficult to modify hardware.
So, please suggest us the sw solution with which the memory can be unlocked via uniflash.
As, this is high priority task for us, looking for a quick response.
Thanks in advance!!!