Part Number: TMS320F280025C
Other Parts Discussed in Thread: CCSTUDIO
I selected New⇒CCS Projects on CCS and created the project test_proj.
Location: C:\test\test_proj
Target: TMS320F280025C
Next, I tried to build test_proj with the following command.
C:\ti\ccs1100\ccs\eclipse\eclipsec.exe -noSplash -data C:\test -ccs.autoImport -application com.ti.ccstudio.apps.projectBuild -ccs. projects test_proj -ccs.configuration Debug
⇒ Failed with the following message.
make clean
Cannot run program "make": Launching failed
Error: Program "make" not found in PATH
After that, I tried to build test_proj with the same command as before without making any changes, and the build succeeded.
(1) I think CCS uses gmake instead of make, so why do I get the above error?
(2) Why did the second build succeed?
Thank you in advance.
Hayao