We're looking to consolidate our device setup, which currently employs two separate microcontrollers. One manages communication protocols and protection functions, while the other controls an LCD display using SCI for command-response communication.
Our aim is to migrate to a TMS320F379D dual-core microcontroller, with Core 1 replacing the first microcontroller's tasks and Core 2 taking over LCD control. We plan to use Inter-Processor Communication (IPC) for core-to-core communication.
Could you recommend IPC examples suitable for our needs? Additionally, we're seeking advice on managing command-response data buffers, which have a size of 100 bytes.