Hello, experts:
I encountered some issues while using the function of coping code from flash to ram. In fact, in the compiler, it is already possible to successfully see that some functions have been placed in RAM space. However, the actual execution time of the test did not decrease.
Compilation also did not report any errors.
The execution time of the code without being placed in RAM is approximately 15 microseconds, while the execution time after being placed in RAM is still around 15 microseconds.