Other Parts Discussed in Thread: C2000WARE, ADS8326
Hello,
I am working on a project with the LAUNCHXL-F28027 and was having trouble changing LOSPCP. Please see the following post for background information:
LAUNCHXL-F28027: Unable to change LOSPCP, resulting in failed SCI transmissions.
In short, solving the LOSPCP problem involved changing clk.c, specifically the CLK_setLowSpdPreScaler() function, rebuilding driverlib, and adding the new driverlib file to my project. With the new driverlib, LOSPCP changes as expected.
After receiving help and succeeding in changing LOSPCP, I noticed that my cpu_timer0_isr is not reached.
I have tried the following to find the source of the problem:
- When I remove the modified driverlib file from the project and add the old driverlib back, cpu_timer0_isr is reached. I am checking that it is reached using a breakpoint in the ISR. When using the modified driverlib file, the breakpoint is never triggered. When using the modified driverlib I can use Step Over all the way from the start of main, successfully reach the while(1) loop, but never trigger the ISR once the while loop is reached.
- While using the modified driverlib, I tried commenting out the
CLK_setLowSpdPreScaler(myClk, CLK_LowSpdPreScaler_SysClkOut_by_1);
line. As expected LOSPCP stays as 0x0002 (the default value) but the ISR still is not reached.
It seems like the problem is due to the modified driverlib file, rather than LOSPCP changing.
Maybe something went wrong when creating the new driverlib file? I'm not sure if this matters, but the pre-modification driverlib file was imported to CCS from
C:\ti\C2000Ware_4_01_00_00\device_support\f2802x\common\ccs,
then the modification to clk.c was made, and finally the modified driverlib file was generated (after rebuilding the driverlib project) in
C:\ti\C2000Ware_4_01_00_00\device_support\common\ccs\Debug
I have copied my main.c function below and included a screenshot of the project folder tree. If it's helpful for me to zip and upload the whole project, I'm happy to do this.
Best Regards,
Oscar
/**
* main.c
* To make things run from flash, I followed the steps in section 2.4.5 of the 'F2802x Firmware Development Package, User's Guide'
*
* This firmware gets a value from the LVDT ADC, then transmits ADC values over UART.
*/
#include "DSP28x_Project.h" // Device Headerfile and Examples Include File (includes stdint.h)
// Include driver header files
#include "f2802x_common/include/adc.h"
#include "f2802x_common/include/clk.h"
#include "f2802x_common/include/gpio.h"
#include "f2802x_common/include/pie.h"
#include "f2802x_common/include/pll.h"
#include "f2802x_common/include/timer.h"
#include "f2802x_common/include/wdog.h"
#include "f2802x_common/include/sci.h"
#include "f2802x_common/include/spi.h"
// Declare function prototype
__interrupt void cpu_timer0_isr(void);
void gpio_setup(void);
void sci_setup(void);
void spi_setup(void);
void spi_fifo_init(void);
// Declare Handles
ADC_Handle myAdc;
CLK_Handle myClk;
GPIO_Handle myGpio;
PIE_Handle myPie;
TIMER_Handle myTimer;
SCI_Handle mySci;
SPI_Handle mySpi;
int main(void)
{
// Declare local handles
CPU_Handle myCpu;
WDOG_Handle myWDog;
PLL_Handle myPll;
// Initialize handles
myAdc = ADC_init((void *)ADC_BASE_ADDR, sizeof(ADC_Obj));
myClk = CLK_init((void *)CLK_BASE_ADDR, sizeof(CLK_Obj));
myCpu = CPU_init((void *)NULL, sizeof(CPU_Obj));
myGpio = GPIO_init((void *)GPIO_BASE_ADDR, sizeof(GPIO_Obj));
myPie = PIE_init((void *)PIE_BASE_ADDR, sizeof(PIE_Obj));
myPll = PLL_init((void *)PLL_BASE_ADDR, sizeof(PLL_Obj));
myTimer = TIMER_init((void *)TIMER0_BASE_ADDR, sizeof(TIMER_Obj));
myWDog = WDOG_init((void *)WDOG_BASE_ADDR, sizeof(WDOG_Obj));
mySci = SCI_init((void *)SCIA_BASE_ADDR,sizeof(SCI_Obj));
mySpi = SPI_init((void *)SPIA_BASE_ADDR, sizeof(SPI_Obj));
// Initialize watchdog handle and disable.
myWDog = WDOG_init((void *)WDOG_BASE_ADDR, sizeof(WDOG_Obj));
WDOG_disable(myWDog);
// Load oscillator calibration values using Device_cal
// According to TRM section 1.3.2.1.2, ADC clocks must be enabled to calibrate the oscillators and ADC parameters.
CLK_enableAdcClock(myClk);
(*Device_cal)();
CLK_disableAdcClock(myClk); //Since the ADC is not needed for this application, it is disabled once calibration is done.
// Set internal oscillator 1 as the clock source.
CLK_setOscSrc(myClk, CLK_OscSrc_Internal);
// Internal oscillator 1 runs at 10MHz, I need 60MHz. Multiply 10MHz by 12, divide by 2
PLL_setup(myPll, PLL_Multiplier_12, PLL_DivideSelect_ClkIn_by_2);
//Disable PIE and all interrupts before changing PIE
PIE_disable(myPie);
PIE_disableAllInts(myPie);
CPU_disableGlobalInts(myCpu);
CPU_clearIntFlags(myCpu);
// Re-enable PIE
PIE_enable(myPie);
// Register interrupt handlers in the PIE vector table
// Group number and subgroup number from TRM Table 1-110.
PIE_registerPieIntHandler(myPie, PIE_GroupNumber_1, PIE_SubGroupNumber_7,
(intVec_t)&cpu_timer0_isr);
#ifdef _FLASH
memcpy(&RamfuncsRunStart, &RamfuncsLoadStart, (size_t)&RamfuncsLoadSize);
#endif
// Configure CPU-Timer 0 to interrupt every 100 milliseconds:
// 60MHz CPU Frequency
TIMER_stop(myTimer);
TIMER_setPeriod(myTimer, (uint32_t)(60 * 100000));
TIMER_setPreScaler(myTimer, 0);
TIMER_reload(myTimer);
TIMER_setEmulationMode(myTimer, TIMER_EmulationMode_StopAfterNextDecrement); //Note this is the default.
TIMER_enableInt(myTimer);
TIMER_start(myTimer);
//Initialize GPIO
gpio_setup();
//Set up SCIA
sci_setup();
//Set up SPI
spi_setup();
spi_fifo_init(); // Initialize the SPI FIFOs
// Enable CPU INT1 which is connected to CPU-Timer 0:
CPU_enableInt(myCpu, CPU_IntNumber_1);
// Enable TINT0 in the PIE: Group 1 interrupt 7
PIE_enableTimer0Int(myPie);
// Enable global Interrupts and higher priority real-time debug events
CPU_enableGlobalInts(myCpu);
CPU_enableDebugInt(myCpu);
while(1){
//Control state of LED D4 using Switch S3
if(GPIO_getData(myGpio, GPIO_Number_12)){
GPIO_setLow(myGpio, GPIO_Number_1);
}
else{
GPIO_setHigh(myGpio, GPIO_Number_1);
}
}
}
void gpio_setup(void){
//LED D2 is connected to GPIO0. Set GPIO0 to GPIO configuration, output direction, and disable pull-up.
GPIO_setMode(myGpio, GPIO_Number_0, GPIO_0_Mode_GeneralPurpose);
GPIO_setDirection(myGpio, GPIO_Number_0, GPIO_Direction_Output);
GPIO_setPullUp(myGpio, GPIO_Number_0, GPIO_PullUp_Disable);
GPIO_setHigh(myGpio, GPIO_Number_0); //Initialize GPIO0 to known state
//LED D4 is connected to GPIO1. Set GPIO1 to GPIO configuration, output direction, and disable pull-up.
GPIO_setMode(myGpio, GPIO_Number_1, GPIO_0_Mode_GeneralPurpose);
GPIO_setDirection(myGpio, GPIO_Number_1, GPIO_Direction_Output);
GPIO_setPullUp(myGpio, GPIO_Number_1, GPIO_PullUp_Disable);
GPIO_setHigh(myGpio, GPIO_Number_1); //Initialize GPIO0 to known state
//LED D3 is connected to GPIO2.
GPIO_setMode(myGpio, GPIO_Number_2, GPIO_0_Mode_GeneralPurpose);
GPIO_setDirection(myGpio, GPIO_Number_2, GPIO_Direction_Output);
GPIO_setPullUp(myGpio, GPIO_Number_2, GPIO_PullUp_Disable);
GPIO_setHigh(myGpio, GPIO_Number_2); //Initialize GPIO0 to known state
//Switch S3 is connected to GPIO12. Set GPIO12 to GPIO configuration, input direction, and disable pull-up.
GPIO_setMode(myGpio, GPIO_Number_12, GPIO_0_Mode_GeneralPurpose);
GPIO_setDirection(myGpio, GPIO_Number_12, GPIO_Direction_Input);
GPIO_setPullUp(myGpio, GPIO_Number_12, GPIO_PullUp_Disable);
}
__interrupt void cpu_timer0_isr(void){
uint16_t txData16 = 0xFFFF;
uint16_t adcData = 0x0000;
uint16_t rxData1 = 0x0000;
uint16_t rxData2 = 0x0000;
//int i = 0;
//Set GPIO0 for debugging/LED
GPIO_setHigh(myGpio, GPIO_Number_0);
//SPI Transmit two 16 bit words to TX FIFO
SPI_write(mySpi,txData16);
SPI_write(mySpi,txData16);
//Wait for 2 words to arrive
while(SPI_getRxFifoStatus(mySpi) != SPI_FifoStatus_2_Words)
{
}
//SPI Read two 16 bit words from RX FIFO
rxData1 = SPI_read(mySpi);
rxData2 = SPI_read(mySpi);
//Combine rxData; discard first 6
adcData = ((rxData1 << 6) & 0xFFC0) | ((rxData2 >> 10) & 0x003F);
//UART Transmit
//Send 16 bit integer as 4 4-bit integers (
//Terminate with line feed "\n"
SCI_putDataBlocking(mySci, (uint8_t)(((adcData & 0xF000) >> 12) + 0x41));
SCI_putDataBlocking(mySci, (uint8_t)(((adcData & 0x0F00) >> 8) + 0x41));
SCI_putDataBlocking(mySci, (uint8_t)(((adcData & 0x00F0) >> 4) + 0x41));
SCI_putDataBlocking(mySci, (uint8_t)(((adcData & 0x000F) >> 0) + 0x41));
SCI_putDataBlocking(mySci, 0x0A); //LF
//Acknowledge interrupt so more interrupts from group 1 can be received.
PIE_clearInt(myPie, PIE_GroupNumber_1);
//Set GPIO0
GPIO_setLow(myGpio, GPIO_Number_0);
}
void sci_setup(void){
//See Example_2802xSci_FFDLB_int.c and TRM section 9.4 for configuration instructions
GPIO_setPullUp(myGpio,GPIO_Number_28,GPIO_PullUp_Enable);
GPIO_setPullUp(myGpio,GPIO_Number_29,GPIO_PullUp_Disable);
GPIO_setQualification(myGpio,GPIO_Number_28,GPIO_Qual_ASync);
GPIO_setMode(myGpio,GPIO_Number_28,GPIO_28_Mode_SCIRXDA);
GPIO_setMode(myGpio,GPIO_Number_29,GPIO_29_Mode_SCITXDA);
//Peripheral registers cannot be modified unless clock to the specific peripheral is enabled.
//Source: Firmware Dev. Package User's Guide, section 2.6.
//Enable clock to SCIA
CLK_enableSciaClock(myClk);
//Set UART Settings. Parity disabled by default.
SCI_disableParity(mySci);
SCI_setNumStopBits(mySci, SCI_NumStopBits_One);
SCI_setCharLength(mySci, SCI_CharLength_8_Bits);
//Enable Rx, Tx, Rx interrupt, Tx interrupt
SCI_enableTx(mySci);
SCI_enableRx(mySci);
//SCI_enableTxInt(mySci); //Not needed.
SCI_enableRxInt(mySci);
//Disable loopback
SCI_disableLoopBack(mySci);
//RX ERR, Sleep, and TXWAKE are disabled by default after system reset.
//Set Baud Rate
//Clock for SCI comes from LSPCLK, which is just SYSCLKOUT divided down according to LOSPCP register, default /4.
//LSPCLK = SYSCLKOUT/(LOSPCP*2) . If LOSPCP = 0, LSPCLK = SYSCLKOUT
//Baud rate = LSPCLK / ((BRR+1)*8), or inverse BRR = (LSPCLK/(Baud*8))-1
//BRR is the 16 bit value stored across SCIHBAUD and SCILBAUD
// SCI BRR = LSPCLK/(SCI BAUDx8) - 1
//Assuming 60MHz clock for F28027 and goal of 9600 Baud, LSPCLK = 60MHz/4 = 15MHz
//BRR = (15MHz/(9600*8))-1 = 194.31 ~ 194
//Back calculate Baud --> (60MHz/4)/((194+1)*8) = 9615.3 Baud, 0.16% error
// SCI_setBaudRate(mySci, (SCI_BaudRate_e)194);
// For 115200, change LOSPCP pre-scaler to /1 for better resolution
//BRR = (60MHz/(115200*8))-1 = 64.10 ~ 64
//Back calculate Baud --> (60MHz)/((16+1)*8) = 115384.61 Baud, 0.16% error
//CLK_setLowSpdPreScaler(myClk, CLK_LowSpdPreScaler_SysClkOut_by_1);
SCI_setBaudRate(mySci, (SCI_BaudRate_e)64);
//Enable SCI
SCI_enable(mySci);
}
void spi_setup(void){
// Initialize GPIO for SPI
GPIO_setPullUp(myGpio, GPIO_Number_16, GPIO_PullUp_Enable);
GPIO_setPullUp(myGpio, GPIO_Number_17, GPIO_PullUp_Enable);
GPIO_setPullUp(myGpio, GPIO_Number_18, GPIO_PullUp_Enable);
GPIO_setPullUp(myGpio, GPIO_Number_19, GPIO_PullUp_Enable);
GPIO_setQualification(myGpio, GPIO_Number_16, GPIO_Qual_ASync); //See TRM 1.4.4.1, SPI peripheral controls synchronization.
GPIO_setQualification(myGpio, GPIO_Number_17, GPIO_Qual_ASync);
GPIO_setQualification(myGpio, GPIO_Number_18, GPIO_Qual_ASync);
GPIO_setQualification(myGpio, GPIO_Number_19, GPIO_Qual_ASync);
GPIO_setMode(myGpio, GPIO_Number_16, GPIO_16_Mode_SPISIMOA);
GPIO_setMode(myGpio, GPIO_Number_17, GPIO_17_Mode_SPISOMIA);
GPIO_setMode(myGpio, GPIO_Number_18, GPIO_18_Mode_SPICLKA);
GPIO_setMode(myGpio, GPIO_Number_19, GPIO_19_Mode_SPISTEA_NOT);
// Set GPIO 32 and 33 to inputs because they are jumped by traces to GPIO 16 and 17
//32 and 33 default to GPIO (see GPBMUX1 register), input direction (GPBDIR), enabled pull-up (GPBPUD).
//Enable clock first to allow change of configuration registers.
CLK_enableSpiaClock(myClk);
//Set SPISWRESET bit, as directed by TRM 8.4.2
//This will also clear the OVERRUN_FLAG and INT_FLAG bits
SPI_reset(mySpi);
// Enable master mode
SPI_setMode(mySpi, SPI_Mode_Master);
SPI_enableTx(mySpi);
//ADC is TI ADS8326, positive edge for DOUT
SPI_setClkPhase(mySpi, SPI_ClkPhase_Normal);
SPI_setClkPolarity(mySpi, SPI_ClkPolarity_OutputFallingEdge_InputRisingEdge);
SPI_setBaudRate(mySpi, SPI_BaudRate_1_MBaud); //DIFFERENT VALUE MIGHT BE NEEDED SINCE ENUM ASSUMES 12.5MHz
//ADC can handle 24kHz to 6MHz. 15/12 = 1.25MHz
// Set 16-bit char bits
SPI_setCharLength(mySpi, SPI_CharLength_16_Bits);
// Release SPI from Reset
SPI_enable(mySpi);
return;
}
void spi_fifo_init()
{
// Initialize SPI FIFO registers
SPI_enableChannels(mySpi);
SPI_enableFifoEnh(mySpi);
SPI_resetTxFifo(mySpi);
SPI_clearTxFifoInt(mySpi);
SPI_resetRxFifo(mySpi);
SPI_clearRxFifoInt(mySpi);
SPI_setRxFifoIntLevel(mySpi, SPI_FifoLevel_4_Words);
}