This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28379D: "Break at address "0x3fe493" with no debug information available, or outside of program code" error due to SysCtl_delay function in sysctl.c file

Part Number: TMS320F28379D

Dear Team,

I am developing the code base with f28379d to interface SCI, CAN, EPWM and internal ADC. However when I added the internal ADC api files; I am unable to debug my code (neither RAM or flash). I get above mentioned error. Sofor more diagnosis i stepped through the code and observed that breakpoint is hitting the ESTOP0 instruction in disassembly window from the line SysCtl_delay(2000); in sysctl.c file. Please help to resolve the issue. I am using only CPU1. Attaching my project in ZIP file for further diagnosis.

CCS Version: 12.6.0.00008
compile version- TI v22.6.1.LTS

Thanks.boost_conv_cpu1.zip

  • Hello Pravin,

    I get above mentioned error

    If this error appears on an opened file when you try to pause the debugging or when it hits an ESTOP0 instruction, this is not an actual issue with the program itself. The message is essentially indicated that it can't find the source file to display it as a normal debugging file (the only way to view the application at this point is to use the Disassembly window). If you want to be able to step through it like a normal file, you will need to include all relevant source files within your project instead of using libraries, that is my understanding.