This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28388D: Can Projects Built with the 379D Build and Run with the 388D?

Part Number: TMS320F28388D


Tool/software:

Greetings,

We have a project which is purely logical (doesn’t use any of the HW resources on the DSP).  It has been running on the 379D.  We would like to be able to use this project, without modification, on the 388D.  But the project properties currently specify the 379D.  Is there any way to have the project get its processor from the main project?  In both cases, the code runs on a C2000 core.  Given that, does it matter?  

Thank you,

Ed