Tool/software:
Hi -
I've ported my firmware from the F28277S 176-pin package to the 100-pin chip. I'm using the strobe line on EQep3 as an axis homing indicator. it is connected to through-beam sensor. GPIO64 is configured/muxed as the EQEP3S line. A signal is seen on the line coming into the processor (and in GPIO64 data), but I'm never seeing the QCFL[SEL] being set. I'm using GPIO62 and GPIO63 as the encoder A and B lines and they are behaving properly. Is there something I should know about EQEP3S on this package? This worked on the 176-pin chip.
Thanks -
Mary