Part Number: TMS320F28388D
Other Parts Discussed in Thread: C2000WARE
Tool/software:
May I ask what is the fastest response time for F28388D slave DC mode PDO communication?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F28388D
Other Parts Discussed in Thread: C2000WARE
Tool/software:
May I ask what is the fastest response time for F28388D slave DC mode PDO communication?
Hi Allen,
First off, the F28388D CAN SW package that is released in C2000Ware does not support higher level protocols, like CANOpen, hence I cannot provide the response time you were inquiring about with respect to PDO communication. You may want to reach out to third party HLP providers (e.g. - Simma Software) as they may have CANOpen solutions for F28388D and may be able to provide this number.
Anyhow, there are two types of CAN that are available in the F28388D device, one type is the classic CAN which is capable of up to 1Mbps and max payload of 8 bytes and the other is CAN-FD which is capable of up to 5Mbps and has a max payload of 64 bytes.
Best regards,
Joseph